... A function that eliminates flickering and reduces the effect of noise in a sharply fluctuating input signal. There are two types of averages that can be used, the simple average and the movi...
...a solid state relay switches between inputting and not inputting a DC voltage. When there is an input voltage, the signal is ON and power is supplied to the heater. When there is no voltage, ...
...te product category Digital Panel Indicators Response of a system to an instantaneous change in input from one constant value to another. The appropriate product category Temperature Controll...
...must-release voltage Definition The appropriate product category Solid-state Relays The maximum input voltage at which the output will change from an ON state to an OFF state. The appropriate...
...Panel Indicators A control loop that uses signals proportional to the linear combination of the input, the time integral of the input, and the time derivative of the input t...
...ollers A measurement of accuracy that indicates if similar results can be obtained for the same input value. Also called the repeatability. The repeat accuracy is different from the accuracy ...
...finition The appropriate product category Solid-state Relays The allowable voltage range of the input signal. The appropriate product category Level Switches The power supply voltage required...
...Model Operation H7AN H7CN Instantaneous output when power is turned ON. Output OFF during reset input. H7BX H7CX In output mode N or F, instantaneous output when power supply is turned ON and...
... are mechanically opened and closed for current switching. Contact Configuration The electrical input/output circuit configuration of contacts which depends on the application. Resin Molding ...