...e appropriate product category Temperature Controllers An active control to compare temperature input signals and provide output regulation to a heating and or cooling process....
...on Programmable Terminals Definition The appropriate product category Programmable Terminals An input device with a touch panel enabling operation on screens created by the user. If you use a...
...ipulated variable. Manual operation is used to output the manipulated variable that is manually input from front-panel keys. Auto/manual switching is used to switch between these....
...unt that serves as the target for feedback control. The abbreviation is SP. If the set point is input with key operations or communications, it’s called the local SP. If the set point is...
...The appropriate product category Counters The ratio between the ON time and OFF time of a count input signal. (The maximum counting speed of a counter is specified at an ON/OFF ratio of 1:1.)...
... Definition The appropriate product category Temperature Controllers The MV to output when a PV input error, RSP input error, or other error occurs....
...on The appropriate product category Timers Operation in which the output turns ON as soon as an input is received and turns OFF after the set time....
...munications software, a modem, or a host computer. An echoback is used to confirm if characters input from a keyboard are transmitted correctly. Echobacks are not performed or are replaced wi...