... the output will not reach L if the mounted phototransistor is mounted near the specified lower limit of light current I L (in this case, near 0.5 mA when I F = 20 mA). (There is variation in...
... of Photomicrosensors built into Equipment? Answer Absolute maximum ratings specify the upper limit of usage conditions for factors such as the voltage, current, temperature, and power. The...
... When performing online editing with the CX-Programmer FA Integrated Tool Package, there is no limit to the number of rungs, but the maximum number of words (number of steps) is limited. If ...
..., what should be done if the result of a BCD double-length addition operation exceeds the upper-limit of double-length data, which is 9999 9999? BCD Double-length Data Range 0 to 9999 9999 No...
...tus changes (i.e., turns ON) and then turn on the work bit for only 1 scan can be used for time limit control between a data output signal and strobe signal in parallel transmissions. Example...
...tus changes (i.e., turns ON) and then turn on the work bit for only 1 scan can be used for time limit control between a data output signal and strobe signal in parallel transmissions. Example...