...method into screw-fastened and snap-in switches. There are also Thumbwheel Switches that have a lock function that locks the set values and prevents them from being changed, as well as Thumbw...
...after it is released. Alternate operation The first time the pushbutton is pressed, an internal lock mechanism holds it in the same position. The next time it is pressed, the lock is...
...s in emergencies, such as when they are welded. • Conforms to EN 60947-5-5. • Includes a safety lock to prevent misuse. • Features separate construction that allows the Switch to be separated...
...itch Unit have been properly mounted can be detected from the open/closed state of the contact (Lock-lever-linked contact function).* * All contacts are interlocked with the lock lev...
...n 7 supply voltage configurations. • Single-function model with ON-delay, OFF-delay, or startup lock settings (SDV-FH[]T). • Select either AC or DC voltage input. • Polarity can be specified ...
...crosshair and shadow masks to be displayed on screen Power input socket equipped with connector lock mechanism to keep power cable firmly in place (supported connector required) Two types of ...
...crosshair and shadow masks to be displayed on screen Power input socket equipped with connector lock mechanism to keep power cable firmly in place (supported connector required) Two types of ...
... Lead Contents FAQ No. FAQ02297 Related Contents Primary Contents Question What is a mechanical lock? Answer A mechanical lock is used in some electromagnetically lock saf...