...g on the nominal voltage. The overvoltage category is one of the factors that decides clearance distance. The nominal voltage is the rated impulse voltage or rated voltage of the component....
...onnectors are specified. There are, however, problems: the transfer speed is slow, the transfer distance is short, communications are easily affected by noise, and only 1-to-1 connections are...
...ed insulation voltage is used as a parameter for dielectric strength tests and for the creepage distance. The rated insulation voltage must always be higher than the rated operating voltage (...
...gle) of a selector switch when it is in the self-holding state. Travel Pretravel PT mm, (°) The distance (or angle) through which the pushbutton moves in going from the free position to the o...
...ck. 2. Not applicable to K7L-UD. Wiring Distances for Sensing Band and Point Sensors The wiring distance depends on the devices that are connected. Check the models of the Sensing Band, Point...
...he speed of sound changes as the air temperature changes, and this results in temperature-based distance measurement error. Reflection and transmission Ultrasound waves move straight forward ...
... device). Refer to Figure 7 below. Connect to ground with a thick line at the shortest possible distance. To let the leakage current escape quickly, and to reduce voltage changes. The wire di...
... move from the free position to the total travel position. Travel Pretravel PT mm, ° The travel distance or angle from the free position to the travel position of the Actuator. Direct Opening...
...rts. 2.The light intensity of a Through-beam model is reduced to 50%, which reduces the sensing distance by about 30%. 3. The Fiber Units listed above have a structure that strongly withstand...