...h-beam, retro-reflective) and color mark sensor. There are 3 products of Photoelectric Sensors. Distance-settable Photoelectric Sensor E3AS-HL / F / L Series E3AS Series changes the “way of u...
...h-beam, retro-reflective) and color mark sensor. There are 3 products of Photoelectric Sensors. Distance-settable Photoelectric Sensor E3AS-HL / F / L Series E3AS Series changes the “way of u...
...n the sensing object and the Sensor. The amount of capacitance varies depending on the size and distance of the sensing object. An ordinary Capacitive Proximity Sensor is similar to a capacit...
...des many varieties of Sensor, including diffuse-reflective, through-beam, retro-reflective, and distance-settable Sensors, as well as Sensors with either built-in or separate amplifiers and F...
...t is increased. This increase in light intensity is used to detect the object. Features Sensing distance ranging from several centimeters to several meters. Easy mounting adjustment. The inte...
...assification What Is a Displacement Sensor? A Displacement Sensor is a device that measures the distance between the sensor and an object by detecting the amount of displacement through a var...
...ron has developed a lineup including both square-shaped type sensor heads with long measurement distance, and ultra-small pen-shaped type (straight or right angle) sensor heads that can be in...
...ed, but only when the high-speed communications mode is used. They cannot be combined when long-distance mode is being used. The two kinds of Slaves cannot be combined in long ...