...change the analog output. Effect of wind Testing conditions: Temperature: 23.5°C, Humidity: 54% Distance (m) Application point of wind Output Value (mA) A B C Near detection surface Middle Ne...
...y Contents Question What is the principle of regular reflection measurements? Answer When the distance of the sensing object changes, the position where the light is received on the receive...
...y Contents Question What is the principle of diffuse reflective measurements? Answer When the distance of the sensing object changes, the position where the light is received on the receive...
...pability of 2 μm should be used. Caution: The resolution does not represent the accuracy of the distance. It indicates reproducibility when positioning a sensing object. The resolution is def...
... Head when the measurement mode is set to the wide mode. The measurement range for the standard distance (measurement distance at center) of the Z500-SW2T is 2.3 mm. Therefore, the w...
...es after performing tests and confirming operation. * Use conditions differ according to wiring distance on the load side, inverter carrier frequency, basic frequency and load status. Since e...
...ms 1 - 10 of 10 Model Number Description E3S-LS3N 0.5M PCB Sensors, Limited Reflective, Sensing distance: 20 to 35 mm, NPN, Without Timer function, Pre-wired model, 0.5 m E3S-LS3N 2M PCB Sens...
...ering the Receiver. (Light may enter even if the Sensors are separated by more than the sensing distance.) If Fiber Units are mounted in opposite each other, slant the Fiber Units as shown in...
...line. A low-frequency radio wave has the tendency to transmit information stably over a greater distance without being affected by variations in terrain due to its long wavelength. Below is a...