... FAQ00411 Related Contents Primary Contents Question What is the principle of operation of Long-distance Proximity Sensor the TL-L Series? Answer The circuit composition and the principle o...
...s in the Proximity Sensor because of the influence of a surrounding metal? Answer The sensing distance is extended, and faulty reset is resulted. Description The sensing distance i...
...d plate is put between the sensor and the noise source (switching power supply). 2) The setting distance of the sensor is separated from the noise source to the place without the influence. W...
...on when using it in the environment where 200G or more magnetic field is generated. The sensing distance extends when the proximity sensor does not turn on, and there is a possibility that fa...
...ve terminal to the switch connection terminals of F92A. In this case, however, the transmission distance will be approximately half the distance when a contact switch is used. If con...
...Contents Question Can a Capacitive Sensor detect charged objects? Answer Yes, but the sensing distance depends on the charged object and the amount of charge. If the object is charged, the ...
...rough-beam or the reflective. When holes are smaller than the lens diameters, the rated sensing distance might not be satisfied because the amount of light decreases. 2. Notes by the sensing ...
...d Contents FAQ No. FAQ00320 Related Contents Primary Contents Question By what principle is the distance-setting Photoelectric Sensor detected? Answer PSD and the dual photodiode are used f...
...ble gives the sensing distances for the Reflectors listed above. Example: E3Z Reflector Sensing distance E39-R1 3 m E39-R1S 4 m E39-R2 5 m E39-R3 1.5 m E39-R9 2.5 m E39-R10 3.5 m E39-RS1 700 ...
...ors, the repeat accuracy is the range of measurement error if the voltage, temperature, sensing distance, sensing object, and angle of the sensing object are the same. E2E Standard Sensors fo...