...nterruption. Diffuse-reflective Sensors may incorrectly detect light incidence, and the sensing distance will decrease.) 2.Photoelectric Sensors cannot be used if the case or lens is immersed...
... depending on the type of light source. Type of light source Transmission rate (%) Installation distance: 1 cm Installation distance: 10 cm Red light (650 to 700 nm) 98.5 86 Infrared...
...wer The amount of light emitted or the amount of light received are adjusted, and the sensing distance is set. (The E3X auto tuning type is excluded.) (1) Through-beam The amount of light r...
...arallel operating range Please confirm parallel operating range on the catalog, install setting distance of adjacent sensor by 1.5 times min. 2. Alternate arrangement setting of photoelectric...
...tical system of the limited reflective sensor, only the regular reflection of a certain limited distance is received because the emitter axis intersects with a receiver axis in the same incli...
...rectionality than E39-R1, so more light returns to the receiver, which enables a longer sensing distance. For reference, the sensing distance for E3Z-R Photoelectric Sensors are 3 m ...
...o, they cannot. If they are used at the same time, the Slit will become tilted, and the sensing distance will be extremely short. Do not use them at the same time. E2E Standard Sensors for De...
...le, however, to use a Slit on only either the emitter or the receiver, depending on the sensing distance and the size of the sensing object. Slits, however, cannot be used on Reflective Photo...
...surface. The anti-fog effect of the coating is similar to that used by ski goggles. The sensing distance with E39-R1K is the same as with E39-R1. For example, with E3Z-R Photoelectric Sensors...
...al coating) Overview of Model Variations Type Ambient temperature range Features Shape, sensing distance (mm)* Model number Through-beam -40°C to 150°C M4 screw 760 E32-T51 -40°C to 200°C L-s...