...an Uninterruptible Power Supply (hereafter called as "UPS") connected to a computer and when an input power supply abnormality (power failure, etc.) occurs, shuts down a computer normally to ...
...es What is a Timer? A timer is a control device that outputs a signal at a preset time after an input signal is received. Top of page Settings and Indications of Timers Example for the H3CR-A...
...e controllers also support JPt. The characteristics of Pt and JPt are different, therefore, the input type of the temperature controller must be correctly set. Compensating Lead Wire Types Th...
... enables simultaneous monitoring of two physical quantities even in equipment using only analog input devices. You can also see the sensor status Self-diagnostic outputs Self-diagnoses the se...
... enables simultaneous monitoring of two physical quantities even in equipment using only analog input devices. You can also see the sensor status Self-diagnostic outputs Self-diagnoses the se...
...nection quality. Sensor I/O Connectors Sensor I/O Connectors are used to convert the wiring for input devices including sensors and actuators into a connector. At workplaces that require a hi...
... 16 Model Number Description K3GN-NDC DC24 1/32 DIN Digital Panel Meter, DC voltage/current/NPN input, Relay contact output K3GN-NDC-FLK DC24 1/32 DIN Digital Panel Meter, DC voltage/current/...
...he CPU Rack. Alternatively, as many as 80 analog I/O points can be used by mounting five Analog Input Units and five Analog Output Units. Improved Refresh Performance for Data Links, Remote I...
...ver fails during a download, the download can be resumed from the point where it was suspended. Input without Wasted Effort! Use Mnemonics to Input Instructions Directly or Use 1-key...