...al-purpose Relays? Answer The distance depends on the type and installation conditions of the cable. Both ends of the Relays coil must measure at least 90% of the rated coil voltage to oper...
... wires or leakage current when Relays is OFF. This may also cause reset failure. Check with the cable manufacturer for how much float capacitance the cables retain. Also check the amount of l...
...graded because of degradation of the internal filling resin, sensing surface resin material, or cable sheath due to ultraviolet light. Stress on Filling Resin Due to Sudden Temperature Change...
...ntents FAQ No. FAQ00402 Related Contents Primary Contents Question Is it possible to extend the cable of the Proximity Sensor? Answer Yes, it provides as follows in each type of the sensor....
...e not subjected to high temperatures. Heat-resistant parts are used for the case, solder, coil, cable and other components of the head section used in high temperatures. These Sensors, howeve...
... above is the same for coaxial and shielded robot cables. Reference Information: For a standard cable, a minimum bending radius of three times cables diameter is recommended. E2E Standard Sen...
...ow can a stored image that is displayed on F160 Vision Sensor be re-measured? Is there a Camera Cable for F150-VS Vision Sensor that can withstand bending? Can the camera cable for t...
... Primary Contents Question Console cables for Vision Sensors can be extended? Answer Standard cable length of the Console "F150-KP" is 2m. Other than this, however, cables of 5m and 10m len...
...hen wiring, be sure not to exceed the maximum possible wiring distances for both the connecting cable and the Sensing Band. Exceeding these distances may lead to faulty operation. Connect one...