...oin two Bands together? Answer 1. The maximum length is 100 m. The possible lengths of sensor cable for a Water Leak Detector (61F-GPN-V50, 61F-WLA) for different lengths of Sensing Bands (...
...ntents Primary Contents Question I'm using General-purpose 61F Floatless Level Controllers with cable conductor of 2 mm2 and a length that is less than 1 km, but it malfunctions. Is there a s...
...wo lock nuts. If the Electrodes are too long, it may cause problems with strength and handling. Cable-type Electrodes (PH) or Electrode Bands are more suitable. Application Model Features and...
...s Primary Contents Question Is it acceptable to wire 61F's Floatless Level Controller electrode cable and power cable in the same duct? Answer There is a possibility of improper op...
...e output current and thus the rising and falling speeds of signals are fast. This allows a long cable distance. They can be connected to open-collector input devices (NPN, PNP). E6C3-CWZ5GH E...
...ead Contents FAQ No. FAQ00969 Related Contents Primary Contents Question How many meters of the cable of the Rotary Encoder are extended? Answer Voltage output and open collector output typ...
... is almost possible by making cut face "D" of the shaft and the direction of drawing out of the cable as the following figure. (within ±15°) E6C3-CWZ[][]H 3. Please confirm ON point of phase ...
...e change of output data and reading timing by becoming long at the rise time of signal when the cable is extended. We recommend the rotary encoder with the strobe signal that informs of readi...
...y from a distance? Answer The distance depends on the type and installation conditions of the cable. Wiring power supplies over a long distance in parallel with power lines may cause reset ...