FAQ01209 for Pressure Sensors | OMRON Industrial A...- ...g this into voltage, ±5% × 1⁄1000 (%) × 4 V (FS) = ±0.2 V, so the line will deviate ±0.2 V max. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions The zero-reset func...
https://www.ia.omron.com/support/faq/answer/35/faq01209/
FAQ01225 for Pressure Sensors | OMRON Industrial A...- ...pressure in a range from -400 to 400kPa is applied within 30 seconds, the sensor is not damaged E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions The zero-reset func...
https://www.ia.omron.com/support/faq/answer/35/faq01225/
FAQ01238 for Pressure Sensors | OMRON Industrial A...- ...it is greater than one atmosphere, and "negative pressure" when it is less than one atmosphere. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions The zero-reset func...
https://www.ia.omron.com/support/faq/answer/35/faq01238/
FAQ01246 for Pressure Sensors | OMRON Industrial A...- ...s equivalent to a pressure of 760 mm-Hg expressed by a height of 760 mm on a mercury barometer. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions The zero-reset func...
https://www.ia.omron.com/support/faq/answer/35/faq01246/
FAQ01297 for Pressure Sensors | OMRON Industrial A...- ...between pressure and output voltage? Answer The relationship is given in the following graph. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions The zero-reset func...
https://www.ia.omron.com/support/faq/answer/35/faq01297/
FAQ01299 for Pressure Sensors | OMRON Industrial A...- ...s. The Pressure Sensor "E8AA Series" can measure it. However, the flow rate cannot be measured. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions The zero-reset func...
https://www.ia.omron.com/support/faq/answer/35/faq01299/
FAQ01316 for Pressure Sensors | OMRON Industrial A...- ... complete absence of air or any objects. It is a condition in which pressure is infinitely low. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions The zero-reset func...
https://www.ia.omron.com/support/faq/answer/35/faq01316/
FAQ01327 for Pressure Sensors | OMRON Industrial A...- ...cm 2 ). How many Pa is 10 kgf/cm 2 ? 1 kgf/cm 2 = 0.0980665 Mpa, so 10 kgf/cm 2 = 0.980665 Mpa. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions The zero-reset func...
https://www.ia.omron.com/support/faq/answer/35/faq01327/
FAQ01340 for Pressure Sensors | OMRON Industrial A...- ...ed, measurement errors and response delays are eliminated, which improves measurement accuracy. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions The zero-reset func...
https://www.ia.omron.com/support/faq/answer/35/faq01340/
FAQ01342 for Pressure Sensors | OMRON Industrial A...- ...le panel and therefore the pressures for four sensors can be controlled from a single location. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions The zero-reset func...
https://www.ia.omron.com/support/faq/answer/35/faq01342/