...G3J-205BL For example, G3J-205BL withstands an inrush current of 150 Apeak. Therefore R > 200 V x √2/150 A = 1.9 Ω Considering the circuit current and ON time, insert the protective resistanc...
...ays can be found using the following equation. Heating value P (W) = Output-ON voltage drop (V) x Carry current (A) For example, if a load current of 8 A flows from G3NA-210B Solid-state Rela...
... pitch, two, 4.3-dia. or M4 holes 47.6 pitch, two 4.3 dia. or M4 holes See note. Dimensions W43 x D68 x H26: G3N-205B, -210B W46 x D71 x H31: G3N-220B W51 ...
...nction saves the internal clock data and settings only, so the output circuit remains OFF. K3HB-X A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current ...
... and Counter's reset input or signal (start) input? Answer The reset input has priority. K3HB-X A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current ...
...lowing Timers support output for a zero set value, provided that operating mode A is used. K3HB-X A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current ...
...o turn the Timer power supply ON/OFF. (Make sure that the contact capacity is sufficient.) K3HB-X A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current ...
...upplying 3 V can be used, but the data backup time depends on the capacity of the battery. K3HB-X A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current ...
...and OFF time are set to zero.) The operations when using the zero settings are as follows: K3HB-X A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current ...
...power supplies from a single input contact or transistor to separate Timers (or Counters). K3HB-X A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current ...