...5 A) S82K-00324 Switch Mode Power Supplies (Input: 100 to 240 VAC, Output: 24 VDC, 0.13 A) K3HB-X A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current ...
...measure the temperature difference between two locations, use two isolated power supplies. K3HB-X A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current ...
...km/h ±0.1 km/h = ±0.1 km/h. Consequently, the display may vary between 84.9 and 85.1 km/h. K3HB-X A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current ...
...'s permissible load resistance > Digital Panel Meter's input resistance × Number of Meters K3HB-X A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current ...
...A. The Shunt is a resistor that converts the DC current to a DC voltage. Setting Examples: K3HB-X A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current ...
... the display is forcibly set to zero. First, restore the auto-zero time to its default setting (X = 9.9999, and Y = 10 E 9). If it is verified that measurements can be taken, set the auto-zer...
...en average processing is not used. Note: The display shows the value measured by sampling. K3HB-X A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current ...
... on the input signal. The number of samples can be selected for the moving average. In the K3HB-X, K3HB-V, K3HB-S, K3HB-H, and K3HB-R Digital Panel Indicators, the number of samples can be se...
... voltage and current. 2. In the case of Analog Signal Input Applicable Digital Panel Meter K3HB-X, K3HB-V, K3HB-S, K3GN, K3MA-J, K3TE, K3TF 3. In the case of Temperature Input Separate a lead...