...upplying 3 V can be used, but the data backup time depends on the capacity of the battery. K3HB-X A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current ...
...inals 3 and 4 for the reset input. A voltage of 2 V or lower is detected as an OFF signal. K3HB-X A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current ...
...als 3 and 4 will be the specified value of 0.5 V when the reset input is ON. Voltage Input K3HB-X A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current ...
...input signals to "H (High)" levels, for the open-collector in the sensor to be turned off. K3HB-X A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current ...
... the Counter cannot be reset. To enable key operations, set the Key Protect Switch to OFF. K3HB-X A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current ...
...ng currents and voltages can be switched. H7BR: 5 V, 2 mA H7HP: 5 V, 2 mA H7EC: 3 V, 20 μA K3HB-X A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current ...
...ignal will not be detected and the input will remain ON, resulting in abnormal operations. K3HB-X A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current ...
...n Can the batteries of the H7E[]-N be replaced? Answer Yes. Applicable Battery: Y92S-36. K3HB-X A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current ...
...of times that EEPROM can be written (i.e., the number of overwrites), however, is limited. K3HB-X A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current ...
...t use no-voltage input? Answer Recommended model: OMRON Solid-state Relay the G3TA-IA/ID K3HB-X A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current ...