...ustrial Automation section Definition The appropriate product category Programmable Controllers A unit of programming used to create, display, and edit programs on the CX-Programmer. Sections...
... constant, but varies from location to location. Ground potential can thus be generated between a device grounded at two different locations. This can cause noise....
...al Automation contact spring Definition The appropriate product category General Purpose Relays A spring for adding contacting force to the contact's contacting section....
...f an alternate action pushbutton when it is in the self-held state, or the position or angle of a selector switch when it is in the self-held state....
...mation MV change rate limit Definition The appropriate product category Temperature Controllers A function that limits the amount of change per unit time in the manipulated variable....
...| OMRON Industrial Automation solar function Definition The appropriate product category Timers A function that turns an output ON and OFF at the stored times for sunrise and sunset in Japan....
...trial Automation solenoid lock Definition The appropriate product category Safety Door Switches A lock on Safety Door Switch with a solenoid lock that operates only when power is app...
...ence Definition The appropriate product category Temperature Controllers An alarm equipped with a function to prevent the alarm from being output if the temperature is already in the specifie...