...Industrial Automation diversity Definition The appropriate product category Wireless Components A radio transmission device can receive signals with one of its two antennas which works better...
...al Automation time sharing Definition The appropriate product category Digital Panel Indicators A technique that is used to run two or more processes concurrently with one processor by altern...
...rial Automation multi-turn absolute Definition The appropriate product category Rotary Encoders A type of rotary encoder that provides information on the accumulated position for more than on...
...Industrial Automation task Definition The appropriate product category Programmable Controllers A unit of a user program the execution of which can be controlled with Task Control In...
...tomation simplex communications Definition The appropriate product category Wireless Components A communications method in which all signals flow in only one direction from a transmi...
...ns until the samples have been taken. There is no relationship to the previously averaged data. A simple average is useful for a long refresh cycle. The number of samples can be set ...
...tion half-duplex communications Definition The appropriate product category Wireless Components A communications method that uses a single frequency to switch transmitting or receivi...
... Industrial Automation repeater Definition The appropriate product category Wireless Components A wireless device installed to increase the communications distance by repeating wireless commu...