...n The appropriate product category Level Switches Water that is free of impurities. It may have a resistance anywhere from 200 kΩ・cm up to 18 MΩ・cm, requiring a super high-sensitiv...
...ll-area wireless communications Definition The appropriate product category Wireless Components A wireless communication available only within a area of 2 to 3 km in radius, such as...
...sition to wastewater."" However, at water treatment plants ""city water"" may refer to water at a stage before it is purified so it has a broader meaning than pure water. "...
...ion where multiple bits of data are simultaneously output, this method outputs data serially on a single transmission line. The use of fewer wires is enabled in this method. The receiving dev...
...oduct category Temperature Controllers The influence on the temperature measurement accuracy of a Temperature Controller caused by the resistance of the compensating leads and other component...
...omation vibration class Definition The appropriate product category Servomotors / Servo Drivers A class based on the value of the vibration measured at the shaft of a motor rotating ...
...the waterworks. Water is delivered to this reservoir from various water sources, passed through a purification plant, and supplied to the residents....
...talled to the outside, dust may enter the device. Take suitable precautions, such as installing a filter. 2) For a Box Fan, the inlet and outlet are specific to each model....