| Site Search | Product Search | IA Global Search |
...riate product category Photoelectric Sensors A Sensor that detects a position from the angle of light reflected from the sensing object to detect the presence or absence of the sensing object...
...elength Definition The appropriate product category Photoelectric Sensors The wavelength of the light source for a Photoelectric Sensor. The following light sources are available: bl...
...uired for the control output to turn OFF after a person enters the detection range for a Safety Light Curtain or Safety Sensor....
...r Lamps Definition The appropriate product category Push Buttons / Indicator Lamps An Indicator light which can signal different output conditions when supplied with a voltage....
...ce and is defined as the illuminance when there is a ±20% change with respect to the value at a light reception output of 200 lx. This is not sufficient to cause malfunction at the operating ...
...it must be mounted to both the emitter and receiver and the sensitivity set to a level at which light can be properly received at the rated detection distance....
...tion The appropriate product category Push Buttons / Indicator Lamps A method in which only the light source of an incandescent lamp model is changed from a filament to an LED and the LED is ...
...spot size Definition The appropriate product category Photoelectric Sensors The diameter of the light beam from a Photoelectric Sensor where it strikes the sensing object....
...countable digits. Display Method The type of element used to display the counting results. LED: Light emitting diode LCD: Liquid crystal display Note:Electromagnetic Counters display results ...
https://www.ia.omron.com/support/guide/11/explanation_of_terms.html
...o Sensors Products Cautions Primary Contents Term Reference diagram Explanation Non-modulated light Modulated light Non-modulated light: Method used to detect ...
https://www.ia.omron.com/support/guide/24/explanation_of_terms.html
... object at an angle θ. With this optical system, the distance range in which regular-reflective light from the object can be detected consistently is the sensing distance. As such, the sensin...
https://www.ia.omron.com/support/guide/43/explanation_of_terms.html
...eflector and the polarizing filters built into the Retro-reflective Sensors to receive only the light reflected from the Retroreflector. The waveform of the light transmitted through...
https://www.ia.omron.com/support/guide/499/further_information.html
...g output, the time required for 10% to 90% change is expressed in terms of the "response time". Light-receiving Element An element used to recognize a laser beam as a signal. There are variou...
https://www.ia.omron.com/support/guide/56/explanation_of_terms.html
...d. Requires partial or complete replacement at the time of inspection. Type 2: No damage except light welding of the magnetic switch. Can remain in use without replacement at the time of insp...
https://www.ia.omron.com/support/guide/753/explanation_of_terms.html
...ad Contents Safety Door Switches Compact Non-contact Door Switches Safety Limit Switches Safety Light Curtains/Safety Sensors Emergency Stop Switches Enabling Switch Safety Controllers Flexib...
...sors English 日本語 Print Page Image Sensing method Distance-setting Sensing distance 35 to 100 mm Light source Red semiconductor laser diode (660 nm) Connection method Pre-wired connector mo...
...sors English 日本語 Print Page Image Sensing method Distance-setting Sensing distance 35 to 250 mm Light source Red semiconductor laser diode (660 nm) Connection method Pre-wired connector mo...
...sors English 日本語 Print Page Image Sensing method Distance-setting Sensing distance 35 to 250 mm Light source Red semiconductor laser diode (660 nm) Connection method Pre-wired connector mo...
...to 35 mm Black paper 80 x 80 mm, installation distance from background: 60 mm min.: 20 to 30 mm Light source Red LED (660 nm) Connection method Pre-wired models Item list of E3S-LS3[] Ratings...
...o 60 mm Black paper 80 x 80 mm, installation distance from background: 120 mm min.: 15 to 50 mm Light source Red LED (660 nm) Connection method Pre-wired models Item list of E3S-LS3[] Ratings...