| Site Search | Product Search | IA Global Search |
...put/Output 2 outputs Power supply voltage 10 to 30 VDC ripple (p-p) 10% included Operation mode Light-ON/Dark-ON selectable Connection method Pre-wired models (Cable length: 2 m) Item list of...
...put/Output 2 outputs Power supply voltage 10 to 30 VDC ripple (p-p) 10% included Operation mode Light-ON/Dark-ON selectable Connection method Pre-wired models (Cable length: 2 m) Item list of...
...upply voltage Supplied from the connector through the Sensor Communications Unit Operation mode Light-ON/Dark-ON selectable Connection method Connector for sensor communications unit Item lis...
...od Retro-reflective with M.S.R. function Sensing distance When using the E39-RP1: 100 to 500 mm Light source Red LED (650 nm) Connection method Pre-wired models Item list of E3ZM-B Ratings/Pe...
...upply voltage Supplied from the connector through the Sensor Communications Unit Operation mode Light-ON/Dark-ON selectable Connection method Connector pre-wired for sensor communications uni...
...upply voltage Supplied from the connector through the Sensor Communications Unit Operation mode Light-ON/Dark-ON selectable Connection method Connector pre-wired for sensor communications uni...
... current Less than 10 mA) Residual voltage: 2 V max. (Load current 10 to 100 mA) Operation mode Light-ON/Dark-ON selectable Protective circuit Output short-circuit protection, Output reverse ...
... current Less than 10 mA) Residual voltage: 2 V max. (Load current 10 to 100 mA) Operation mode Light-ON/Dark-ON selectable Protective circuit Output short-circuit protection, Output reverse ...
... current Less than 10 mA) Residual voltage: 2 V max. (Load current 10 to 100 mA) Operation mode Light-ON/Dark-ON selectable Protective circuit Output short-circuit protection, Output reverse ...
... current Less than 10 mA) Residual voltage: 2 V max. (Load current 10 to 100 mA) Operation mode Light-ON/Dark-ON selectable Protective circuit Output short-circuit protection, Output reverse ...
... current Less than 10 mA) Residual voltage: 2 V max. (Load current 10 to 100 mA) Operation mode Light-ON/Dark-ON selectable Protective circuit Output short-circuit protection, Output reverse ...
...d to the workpiece. And then the emission power is adjusted to optimize the amount of dispersed light that is received. Stable Detection with Triangulation With triangulation, the workpiece i...
... indicator is installed for each monitor point on a panel or control console. An indicator will light and a bell will sound when an error occurs in the process....
...models are available, including Slot-type Sensors (through-beam) for non-modulated or modulated light, Reflective Sensors, and Sensors with separate emitters and receivers. Introduction Featu...
https://www.ia.omron.com/support/guide/24/further_information.html
...inclination of the object. In the case of (B) and (C), stray reflectons occur and the reflected light is not uniform, however, the effect of inclination is small. E4B Rectangular Ultrasonic P...
https://www.ia.omron.com/support/guide/55/further_information.html
...(the exact angle depends on the model), the amount of error increases due to regular-reflective light in relation to the optical axis of the Sensor. This affects Diffuse-reflective Sensors on...
https://www.ia.omron.com/support/guide/56/further_information.html
...h Standards Certification FAQ Power Supplies / In Addition Glossary of Industrial Automation UV-Light Curing Systems Item A to Z Index Features Lineup Specifications Dimensions Catalog Catalo...
https://www.ia.omron.com/products/family/1876/download/catalog.html
...tons to achieve both cost reduction and improved click feeling. Revised user interface The L/D (Light on / Dark on) button present on conventional models is eliminated, reflecting customer op...
...rom black polished workpieces (such as the painted surface of a car body), which reflect little light, to metal workpieces, which reflect a lot of light. Wide angle characteristic en...
...ntribute to predicting and preventing future events. With these Separate-amplifier Sensors, the light from the Amplifier is transmitted through a fiber to enable detection in narrow places, o...