| Site Search | Product Search | IA Global Search |
...nsor E2Q6. June 1, 2015 We have introduced Rectangular Proximity Sensor E2Q6. Freely Change the Sensing Direction Change between any of five sensing directions: front or 90° up, down...
...1 - 18 of 18 Model Number Description E2E-X10B4-IL2 2M IO-Link Proximity Sensor, Shielded, M30, Sensing distance: 10 mm, DC 3-wire, PNP output, COM2 (38.4 kbps), Pre-wired model, 2 m E2E-X10B...
...scription E2EQ-X10B4-IL2 2M IO-Link Proximity Sensor (Spatter-resistant Models), Shielded, M30, Sensing distance: 10 mm, COM2 (38.4 kbps), Pre-wired model, 2 m E2EQ-X10B4-IL2 5M IO-Link Proxi...
...ts. Machines can be developed to enhance strength by leveraging cooling performance data. Multi-sensing technology [Flow rate] Uses the "Thermal flow rate measurement algorithm". The sensor c...
...dispensing pressure without relying on the experience or skills of maintenance personnel. Multi-sensing technology [Pressure] Uses a piezoelectric element. Since the sensing surface ...
...mber Description E3JM-10M4-G-NN Photoelectric Sensor, AC/DC Power-free type, Through-beam type, Sensing distance: 10 m, Relay output, Conduit: PG13.5 E3JM-10M4-NN Photoelectric Sensor, AC/DC ...
...er Description E2EQ-X10D1 2M Spatter-resistant Proximity Sensor, Standard model, Shielded, M30, Sensing distance: 10 mm, DC 2-wire, NO, Pre-wired model, 2 m E2EQ-X10D1 5M Spatter-resistant Pr...
...f 16 Model Number Description E2FQ-X10D1 2M Chemical-resistant Proximity Sensor, Shielded, M30, Sensing distance: 10 mm, DC 2-wire, NO, Pre-wired model, 2 m E2FQ-X10D1 5M Chemical-resistant P...
... 16 Model Number Description E2K-C20MC1 2M Long-distance Proximity Sensor, 34 dia., Unshielded, Sensing distance: 20 mm, Noise immunity type, DC 3-wire, NPN, NO, Pre-wired model, 2 m E2K-C20M...
...19 of 19 Model Number Description E3Z-G61 0.5M Grooved type photoelectric sensor, Grooved Type, Sensing distance: 25 mm, NPN open collector, 1 axes, Pre-wired model, 0.5 m E3Z-G61 2M Grooved ...
...er Description E3Z-LS61 0.5M Compact Photoelectric Sensor with Built-in Amplifier, Square type, Sensing distance: 20 to 200 mm (BGS max setting), NPN open collector, Pre-wired model, 0.5 m E3...
...- 16 of 16 Model Number Description EE-SPX302-W2A 1M Photomicrosensor, Slot type, Through-beam, Sensing distance: 3.6 mm (slot width), Dark-ON, NPN output, Pre-wired model, 1 m EE-SPX302-W2A ...
... detection by Muting Sensors A and B. Adjust where Muting Sensors A and B are installed and the sensing direction so that the passage of a person does not interrupt the beams from both Sensor...
...perture angle (directional angle) listed in the catalog specifications is within ±2.5° when the sensing distance for the emitter and receiver is at least 3m. This means that the effective ape...
...ated of Photomicrosensors Used for Industrial Equipment? Answer The following table shows the sensing method and characteristics for modulated and non-modulated light. Non-modulated Modulat...
...s (EE-SX[][][]A,[][][]R) with operation indicators that are lit when light is interrupted (when sensing objects are detected) are available. *1. The Dark-ON⁄Light-ON (selectable) models are n...
... Sensors Lead Contents FAQ No. FAQ01184 Related Contents Primary Contents Question What are the sensing position characteristics of Slot-type Photomicro Sensors? Answer See the following di...
... Sensors with a Slit on the light emitting/receiving window. Reference information: Because the sensing performance of Photomicro Sensors does not have a margin as wide as that for Photoelect...
...the following values as a guide. Slot-type Photomicro Sensors: Approx. 0.025 to 0.05 mm (If the sensing object travels across the shorter side of the light emitting/receiving window.) Reflect...
...ions of the slit for slot-type Photomicro Sensors? Answer It is the same size as the standard sensing object given in the catalog. Example: Standard opaque sensing object measuring...