Primary Contents

IA Global Search Results

Select Country in

Site Search Product Search IA Global Search
Results 3901 - 3920 of 19082
faq02149

...spring is a single wire, the rod flexes considerably. Use WLNJ when the arrival position of the sensing object fluctuates. The flexibility of the rod, however, causes gaps to appear in the co...

https://www.ia.omron.com/support/faq/answer/30/faq02149/

FAQ00691 for Level Switches | OMRON Industrial Aut...

...en the terminals, and that there is no danger of a ground fault in the cables or Liquid Leakage Sensing Bands. Note:For explosion-proof areas, use F03-20 Liquid Leakage Sensor, which has been...

https://www.ia.omron.com/support/faq/answer/33/faq00691/

FAQ00692 for Level Switches | OMRON Industrial Aut...

...No. FAQ00692 Related Contents Primary Contents Question How long is your longest Liquid Leakage Sensing Band? Also, how do you join two Bands together? Answer  1. The maximum length is 100 m...

https://www.ia.omron.com/support/faq/answer/33/faq00692/

FAQ00848 for Level Switches | OMRON Industrial Aut...

...Level Controllers "61F" does not work even if it is powered on and the liquid level reaches the sensing level. What may be the reason for it? Answer  Check the following points. (1) Are ther...

https://www.ia.omron.com/support/faq/answer/33/faq00848/

FAQ01855 for Push Buttons / Indicator Lamps | OMRO...

...ion was confirmed by performing the tests described in the table below and making sure that the sensing distance and installation resistance satisfied the performance specifications after rep...

https://www.ia.omron.com/support/faq/answer/38/faq01855/

FAQ00201 for Proximity Sensors | OMRON Industrial ...

...imity Sensor occur? Answer  For the proximity sensor, when there are the metals other than the sensing object circumferentially, the oscillation that decreases when the sensing obje...

https://www.ia.omron.com/support/faq/answer/41/faq00201/

FAQ00302 for Proximity Sensors | OMRON Industrial ...

...nt is generated on the metal surface by the metal's approaching the oscillation coil built into sensing surface, and the impedance of the detector coil changes by the electromagnetic inductio...

https://www.ia.omron.com/support/faq/answer/41/faq00302/

FAQ00308 for Proximity Sensors | OMRON Industrial ...

...are notes in the idea of the repeat accuracy of the Proximity Sensor? Answer  Factors that the sensing distance or area of the proximity sensor changes are an ambient temperature and an oper...

https://www.ia.omron.com/support/faq/answer/41/faq00308/

faq00311

... V when A turns ON, and the load current will flow through A causing random operation. When the sensing object approaches B, the voltage of both terminals of B is too low at 10 V and the swit...

https://www.ia.omron.com/support/faq/answer/41/faq00311/

faq00314

...appens if Proximity Sensors are used in high temperatures? Answer  The change in the specified sensing distance will be larger than the specified value if Proximity Sensors are used at a tem...

https://www.ia.omron.com/support/faq/answer/41/faq00314/

faq00348

...180°. However, install it so that the direction of travel is in the direction of the arrow. The sensing distance will decrease if the magnet section is mounted on a steel plate or other magne...

https://www.ia.omron.com/support/faq/answer/41/faq00348/

faq00380

...nce) of Proximity Sensors may be degraded because of degradation of the internal filling resin, sensing surface resin material, or cable sheath due to ultraviolet light. Stress on Filling Res...

https://www.ia.omron.com/support/faq/answer/41/faq00380/

FAQ00388 for Proximity Sensors | OMRON Industrial ...

...E Series and TL Series, etc.), please consider that DC/AC magnetic field is 200G or less on the sensing surface of sensor when the sensor is installed. If it is 200G or less, it is possible t...

https://www.ia.omron.com/support/faq/answer/41/faq00388/

FAQ00391 for Proximity Sensors | OMRON Industrial ...

... Question What is "NO (normal open)"? What is "NC (normal close)"? Answer  NO: When there is a sensing object within sensing range, transistor output is ON. NC: When there is not a ...

https://www.ia.omron.com/support/faq/answer/41/faq00391/

FAQ00397 for Proximity Sensors | OMRON Industrial ...

...tion depending on the capacitance change of this electrode is composed, and the approach of the sensing object is detected by increase of the oscillation amplitude. When the sensing ...

https://www.ia.omron.com/support/faq/answer/41/faq00397/

FAQ00402 for Proximity Sensors | OMRON Industrial ...

...mplifier is changed, the oscillation frequency is changed, and the characteristic change in the sensing distance and the temperature characteristic occurs. Therefore, it is not warrantable th...

https://www.ia.omron.com/support/faq/answer/41/faq00402/

FAQ00411 for Proximity Sensors | OMRON Industrial ...

...etic field' is caused in a detector coil 2 by generating the eddy current on the surface of the sensing object when the sensing object approaches. Detector coil 1: Only 'Magnetic fie...

https://www.ia.omron.com/support/faq/answer/41/faq00411/

FAQ00412 for Proximity Sensors | OMRON Industrial ...

...0412 Related Contents Primary Contents Question What is "Response frequency"? Answer  When the sensing object moves at high speed and it passes continuously, the response of proximity sensor...

https://www.ia.omron.com/support/faq/answer/41/faq00412/

FAQ00416 for Proximity Sensors | OMRON Industrial ...

...on occurs in the Proximity Sensor because of the influence of a surrounding metal? Answer  The sensing distance is extended, and faulty reset is resulted. Description The sensing di...

https://www.ia.omron.com/support/faq/answer/41/faq00416/

FAQ00417 for Proximity Sensors | OMRON Industrial ...

...g (2) It remains the state when the sensor detects the object regardless of the presence of the sensing object. (2) It remains the state when the sensor detects the object regardless of the p...

https://www.ia.omron.com/support/faq/answer/41/faq00417/

Results 3901 - 3920 of 19082

Select Country in