Primary Contents

IA Global Search Results

Select Country in

Site Search Product Search IA Global Search
Results 3921 - 3940 of 19082
FAQ00418 for Proximity Sensors | OMRON Industrial ...

...operation The aluminum chips with small density are not detected, and the detection only of the sensing object is enabled by setting the oscillation frequency lower than usually though it is ...

https://www.ia.omron.com/support/faq/answer/41/faq00418/

FAQ00434 for Proximity Sensors | OMRON Industrial ...

...he TL Series excluding the TL-L100 Series, etc.) If DC/AC magnetic field is 200G or less on the sensing surface of sensor, it is possible to use it. The proximity sensor cannot oscillate and ...

https://www.ia.omron.com/support/faq/answer/41/faq00434/

FAQ01074 for Proximity Sensors | OMRON Industrial ...

... FAQ01074 Related Contents Primary Contents Question What is "Response time"? Answer  When the sensing object moves at high speed and it passes continuously, the response of proximity sensor...

https://www.ia.omron.com/support/faq/answer/41/faq01074/

faq02657

...ors, which reduces the influence of surrounding metal. As shown in Figure 2, the surface of the sensing coil on Unshielded Proximity Sensors is not covered with metal, so flux is also generat...

https://www.ia.omron.com/support/faq/answer/41/faq02657/

faq03386

...Primary Contents Question Can a Capacitive Sensor detect charged objects? Answer  Yes, but the sensing distance depends on the charged object and the amount of charge. If the object is charg...

https://www.ia.omron.com/support/faq/answer/41/faq03386/

FAQ00227 for Photoelectric Sensors | OMRON Industr...

...iameter basically. Please refer to the following so that the idea is different depending on the sensing method. 1. Idea to use the light through the hole Please make the hole of the same size...

https://www.ia.omron.com/support/faq/answer/43/faq00227/

FAQ00320 for Photoelectric Sensors | OMRON Industr...

...  PSD and the dual photodiode are used for the light receiving element and the distance to the sensing object is judged by detecting the reflected light spot position on the light receiving ...

https://www.ia.omron.com/support/faq/answer/43/faq00320/

faq00335

...R, E3S-CR62/67, E32-R21, and E32-R16) or to the E3T. Explanation: The following table gives the sensing distances for the Reflectors listed above. Example: E3Z Reflector Sensing dist...

https://www.ia.omron.com/support/faq/answer/43/faq00335/

faq00381

...ric Sensors, the repeat accuracy is the range of measurement error if the voltage, temperature, sensing distance, sensing object, and angle of the sensing object are the sam...

https://www.ia.omron.com/support/faq/answer/43/faq00381/

faq00401

... light interruption. Diffuse-reflective Sensors may incorrectly detect light incidence, and the sensing distance will decrease.) 2.Photoelectric Sensors cannot be used if the case or lens is ...

https://www.ia.omron.com/support/faq/answer/43/faq00401/

FAQ00413 for Photoelectric Sensors | OMRON Industr...

...sor? Answer  The amount of light emitted or the amount of light received are adjusted, and the sensing distance is set. (The E3X auto tuning type is excluded.) (1) Through-beam The amount of...

https://www.ia.omron.com/support/faq/answer/43/faq00413/

FAQ00422 for Photoelectric Sensors | OMRON Industr...

...ng alternative arrangement. Condition: The light of the next emitter might be received when the sensing object is close to the photoelectric sensor. 3. Use of mutual interference prevention f...

https://www.ia.omron.com/support/faq/answer/43/faq00422/

faq02678

...y and directionality than E39-R1, so more light returns to the receiver, which enables a longer sensing distance. For reference, the sensing distance for E3Z-R Photoelectric Sensors ...

https://www.ia.omron.com/support/faq/answer/43/faq02678/

faq02949

...swer  No, they cannot. If they are used at the same time, the Slit will become tilted, and the sensing distance will be extremely short. Do not use them at the same time. E2E Standard Sensor...

https://www.ia.omron.com/support/faq/answer/43/faq02949/

faq03125

...c Sensors to decrease the lens diameter and narrow the light beam. This is done to increase the sensing performance for the smallest detectable object. Usage One set of two Slits for the emit...

https://www.ia.omron.com/support/faq/answer/43/faq03125/

faq03147

...lective surface. The anti-fog effect of the coating is similar to that used by ski goggles. The sensing distance with E39-R1K is the same as with E39-R1. For example, with E3Z-R Photoelectric...

https://www.ia.omron.com/support/faq/answer/43/faq03147/

faq03192

... it be corrected? Answer  Retroreflective Sensors normally have the MSR function, and so shiny sensing objects can also be detected. Perform a test before using Sensors for sensing ...

https://www.ia.omron.com/support/faq/answer/43/faq03192/

faq03418

...SUS spiral coating) Overview of Model Variations Type Ambient temperature range Features Shape, sensing distance (mm)* Model number Through-beam -40°C to 150°C M4 screw 760 E32-T51 -40°C to 2...

https://www.ia.omron.com/support/faq/answer/43/faq03418/

faq00849

..., it can. It is possible to detect more than one liquid leakage with a single K7L by connecting sensing bands in parallel with use of terminal blocks However, be aware that the ...

https://www.ia.omron.com/support/faq/answer/48/faq00849/

FAQ01249 for Ultrasonic Sensors | OMRON Industrial...

...nfiguration of objects detected by the Ultrasonic Sensors? Answer  Types and configurations of sensing objects(Reflective Type) Types and configurations of sensing objects are divid...

https://www.ia.omron.com/support/faq/answer/50/faq01249/

Results 3921 - 3940 of 19082

Select Country in