| Site Search | Product Search | IA Global Search |
... high (guideline: 10 to 15 years). The electrolyte is highly corrosive, and is also conductive, so there is a risk not only of corrosion of peripheral components, but also emission of smoke a...
https://www.omron-ap.com.ph/data_pdf/cat/timer_replace_tg_e_1_1_csm1062339.pdf
... high (guideline: 10 to 15 years). The electrolyte is highly corrosive, and is also conductive, so there is a risk not only of corrosion of peripheral components, but also emission of smoke a...
https://www.omron.co.id/data_pdf/cat/timer_replace_tg_e_1_1_csm1062339.pdf
... high (guideline: 10 to 15 years). The electrolyte is highly corrosive, and is also conductive, so there is a risk not only of corrosion of peripheral components, but also emission of smoke a...
https://www.omron.com.au/data_pdf/cat/timer_replace_tg_e_1_1_csm1062339.pdf
... high (guideline: 10 to 15 years). The electrolyte is highly corrosive, and is also conductive, so there is a risk not only of corrosion of peripheral components, but also emission of smoke a...
https://www.omron.com.vn/data_pdf/cat/timer_replace_tg_e_1_1_csm1062339.pdf
...ns or safety output functions. There are 1 products of Safety I/O Unit. Safety I/O Unit NX-SI / SO Build a simple and flexible safety system...
...trial Automation Other Units Other Units List Other Units are available for expansion racks and so on. There are 1 products of Other Units. CJ-series I/O Control Unit / I/O Interface Unit CJ1...
...for a load that exceeds the contact ratings of the Relay, such as the switching capacity. Doing so may result in reducing Relay performance for insulation failure, contact welding, and contac...
https://www.ia.omron.com/product/cautions/17/precautions_for_safety_use.html
...for Correct Use Operation Key Use only the designated Operation Key. The Head has been designed so that operation is not possible with a screwdriver or other tools. Using anything other than ...
https://www.ia.omron.com/product/cautions/21/precautions_for_correct_use.html
...is affected by the condition of the reflection surface of the detected object. Mount the sensor so that the ultrasound beam is perpendicular to the reflection surface. Obstacles around the se...
https://www.ia.omron.com/product/cautions/55/precautions_for_correct_use.html
...mercial power supply frequency. In Japan, the commercial power supply frequency is 50 or 60 Hz, so the power supply harmonics are, for example, double or triple that frequency, i.e., 100 and ...
...OFF angle settings for the cam. Cam Protection Protection that can be set for each bank and cam so that the cam ON/OFF angle settings will not be accidentally changed or deleted. Test Operati...
https://www.ia.omron.com/support/guide/12/explanation_of_terms.html
... Type Two materials with transparent conductive layers (ITO) are placed with a gap between them so that transparent conductive layers are facing each other. When the touch panel is pressed do...
https://www.ia.omron.com/support/guide/27/further_information.html
...ndards. When the quality of the barcode printing is not good, the data may be read incorrectly, so it is important to take care in printing labels etc. Features of Barcodes Highly flexibility...
...ndards. When the quality of the barcode printing is not good, the data may be read incorrectly, so it is important to take care in printing labels etc. Features of Barcodes Highly flexibility...
https://www.ia.omron.com/support/guide/349/introduction.html
...g cable length of 120 meters. This corresponds to a wiring cable length of 150 max. in Table 2, so the maximum length of Sensing Band that can be connected is 150 meters. Example: Parallel Co...
https://www.ia.omron.com/support/guide/48/further_information.html
...D40A-2 ● D40A *1. Use the D40A-2 and D40A in combination with the G9SX-NS/NSA ,G9SP or NX-SL/SI/SO. Note: Contact your OMRON representative if Applicable Standard No.and Certification Body ar...
...-2*1 ● D40A*1 *1. Use the D40A-2 and D40A in combination with the G9SX-NS/NSA ,G9SP or NX-SL/SI/SO. Note: Contact your OMRON representative if Applicable Standard No. are required. Top of pag...
... Not applicable ● D40A*1 *1. Use the D40A in combination with the G9SX-NS/NSA, G9SP or NX-SL/SI/SO. Note: Contact your OMRON representative if Applicable Standard No.and Certification Body ar...
... high (guideline: 10 to 15 years). The electrolyte is highly corrosive, and is also conductive, so there is a risk not only of corrosion of peripheral components, but also emission of smoke a...
https://www.omron.com.tw/data_pdf/cat/timer_replace_tg_e_1_1_csm1062339.pdf
...g position Angle adjustment up to 330° After fastening to the adapter, you can adjust the angle so that the display is easy to see. 180° reverse display The display can rotate 180°. Useful fu...