Site Search | Product Search | IA Global Search |
...e following characters can be used as wild cards. *: Wild card of a text string that includes 0 digit. ?: Single-character wild card ASCII code table: p. 52 1 Press an unused inspection item ...
https://www.fa.omron.com.cn/data_pdf/mnu/z315-e1-01_fq-cr1.pdf
... Press [Back]. Saved Log Data •Storage Locations and File Names for Logged File Data *1: A five-digit number is assigned as a name to the image data storage folder in the order of folder crea...
https://www.fa.omron.com.cn/data_pdf/mnu/z316-e1-02_fq-cr.pdf
... occur.) 9 - Do not set. (A mode setting error will occur.) Item Description Setting method Two-digit decimal number The left rotary switch sets the 10s digit, and the right rotary s...
https://www.fa.omron.com.cn/data_pdf/mnu/z320-e1-06_v680-ham42-prt.pdf
...e following characters can be used as wild cards. *: Wild card of a text string that includes 0 digit. ?: Single-character wild card ASCII code table: p. 54 1 Press an unused inspection item ...
https://www.fa.omron.com.cn/data_pdf/mnu/z329-e1-02_fq-cr1_____-m.pdf
...this function, bar codes can be read from any angle. Curvature In the following conditions, 12-digit UPC codes can be read within a range of R 20. •Code: 12-digit UPC, resolution = ...
https://www.fa.omron.com.cn/data_pdf/mnu/z333-e1-04_v400-r2.pdf
...rd: 12 or 13 times or more of the narrow bar width) 8. To improve reading reliability •When the digit is determined, designate the digit to use the bar code. •Use the modulus check (...
https://www.fa.omron.com.cn/data_pdf/mnu/z334-e1-03_v500-r2.pdf
... Start Input = bit 1 EDM Input = bit 2 7 Seven Segment Display Data Type: UINT 16-bit 11 (0x0B) Digit Low followed by Digit High Each Digit Displays 1 to 9 (0x01 to 0x09) fo...
https://www.fa.omron.com.cn/data_pdf/mnu/z336-e1-07_os32c-dm.pdf
...e the text string "2014/01/01," enter "2014/01/01" in the string format area. To recognize four-digit numbers, enter as [####], where each "#" represents a number, in the string format area. ...
https://www.fa.omron.com.cn/data_pdf/mnu/z337-e1-12_fq2-s_ch.pdf
...0 PLC Link EtherNetI/P, PROFINET Year data: 1900 to 2100 Response data •6CH 7 to 0 bit: year (2-digit year) or time •6CH 15 to 8 bit: month or minute •7CH 7 to 0 bit: day or second •7CH 15 to...
https://www.fa.omron.com.cn/data_pdf/mnu/z338-e1-05_fq2-s_ch.pdf
...her Reader/Writer (B). p.175 2 words (4 bytes) Overwrite count control area Always 00 hex Lower digit Middle digit Upper digit 110 Section 6 RF Tag Communications RFID Syste...
https://www.fa.omron.com.cn/data_pdf/mnu/z339-e1-17_v680s-hmd6_-etn.pdf
...0 max [ Unit : mm ] < Screw: M5 or M6 > F3SG-RA-30 Series Dimension A C1+18 Dimension C1 4-digit...
https://www.fa.omron.com.cn/data_pdf/mnu/z352-e1-11_f3sg-_r_.pdf
...her Reader/Writer (B). p.165 2 words (4 bytes) Overwrite count control area Always 00 hex Lower digit Middle digit Upper digit Section 6 RF Tag Communications Section 6 Func...
https://www.fa.omron.com.cn/data_pdf/mnu/z353-e1-15_v680s-hmd6_-eip.pdf
...mware Version of Node 1 The response code (00: normal) and firmware version are returned as a 4-digit decimal number. * The above response is for a firmware version of 1.00. SOH Node No. Comm...
https://www.fa.omron.com.cn/data_pdf/mnu/z360-e1-05_v640-ham11-v4_-l-v2.pdf
...rsion of Amplifier Unit The response code (00: normal) and firmware version are returned as a 4-digit decimal number. * The above response is for a firmware version of 1.00. Example 3: Gettin...
https://www.fa.omron.com.cn/data_pdf/mnu/z361-e1-07_v640-ham11(-l)-etn-v2.pdf
...* Serial number format @@@@@@@ (1)(2)(3)(4)(5)(6)(7) Software: Firmware version is 2.1 or later Digit Meaning Displayed characters (1) Sequential number from 0001 0001 to 9999 (2) (3) (4) (5)...
https://www.fa.omron.com.cn/data_pdf/mnu/z362-e1-09_zw-_000.pdf
...is based on the object dictionary of the CAN application protocol. All objects are assigned a 4-digit hex index and comprise the following areas. Data type The following data types are used b...
https://www.fa.omron.com.cn/data_pdf/mnu/z363-e1-07_zw-_000.pdf
...ive number = inverting all bits of a positive number and then adding 1 to the result. The first digit is used to judge whether the number is positive or negative. •When 0: Positive number (or...
...ive number = inverting all bits of a positive number and then adding 1 to the result. The first digit is used to judge whether the number is positive or negative. •When 0: Positive number (or...
...ax [ Unit : mm ] < Screw: M5 or M6 > F3SG-4RA-25-01TS Series Dimension A C+23 Dimension C 4-digit...
https://www.fa.omron.com.cn/data_pdf/mnu/z380-e1-04_f3sg-4ra____-25-01ts.pdf
...ate this bracket at half the Dimension C (or at the center of the sensor length). Dimension C 4-digit number of the type name (Protective height) Dimension D C-20 Dimension P F3SG-4RR□□□□-14 ...
https://www.fa.omron.com.cn/data_pdf/mnu/z383-e1-04_f3sg-_rr.pdf