| Site Search | Product Search | IA Global Search |
...r operation floating blanking function flowrate force necessary to reverse the direction of the lever force-set/reset forward forward and reverse drive prohibit forward current forward voltag...
...dder language Ladder Monitor Ladder Support Pack20 lamp last maintenance date function latching lever LBA LBA detection band leakage current leakage current characteristic leakage inductance ...
...s only) added to enable opening contacts when faults occur, such as fused contacts. • Safety of lever settings ensured using a mechanism that engages a gear between the operating position ind...
...elay Saves Space in Panel General-purpose Relays MK-S New Super MK Relays. Models with Latching Lever Added to the Series. Power Relay MM Stable Contact Reliability and Long Life Latching Rel...
https://www.ia.omron.com/products/category/relays/general-purpose-relays/for-control-panel/
...h a 22.3-mm diameter. The Switch Unit and Operation Unit are connected and disconnected using a lever. Both Knob-type and Key-type Selector Switches as well as Indicators are available. There...
https://www.ia.omron.com/products/category/switches/push-buttons_indicator-lamps/phi22-phi25-type/
...Switch Offers Choice of Many Actuators Miniature Limit Switch D4CC Many Models Including Roller Lever Switches are Only 16-mm Thick with Connector General-purpose Limit Switch HL-5000 Economi...
https://www.ia.omron.com/products/category/switches/limit-switches/general-purpose-vertical/
...mber Description D4N-1120 Safety Limit Switch, PG13.5, 1-conduit, 1NC/1NO (snap-action), Roller lever (resin lever, resin roller) D4N-1122 Safety Limit Switch, PG13.5, 1-conduit, 1NC...
...Unit have been properly mounted can be detected from the open/closed state of the contact (Lock-lever-linked contact function).* * All contacts are interlocked with the lock lever. (...
... set using the adjustment dial. According with that, the operating distance between the release lever and shifter is set. On the other hand, the current flows through the heater that composin...
https://www.ia.omron.com/support/guide/753/introduction.html
...纖感應器/出線型/NPN輸出 促銷價 760 元 EE-SX771 2M (原價525) 對照型(溝槽型)/ 出線型 / NPN輸出 促銷價 340 元 WL-9H100(WLNJ HEAD.LEVER) (原價240) 單品零件/頭部單品/螺旋彈簧型 促銷價 170 元 E2E...
...-S General-purpose Relays General-purpose Relays MK-S New Super MK Relays. Models with Latching Lever Added to the Series. Displaying individual registered product index. Select and click for...
...imit Switches Lead Contents FAQ No. FAQ02077 Related Contents Primary Contents Question Can the lever of a WL General-purpose Limit Switch be mounted on WLF2 Explosion-proof Limit Switch? Ans...
...tents Question Can the actuator of WL Limit Switch be mounted on other Limit Switches? Answer Lever actuators can be mounted on the following models. Applicable models: HL Limit Switch, D4C...
...ferences between WL[][]-2 Limit Switch and WL[][]-2N Limit Switch ? Answer The WL[][]-2 has a lever with 90 ° operation to each side, with one-side operation not possible, and a Head that c...
...on TZ-1G High-temperature Basic Switch, Pin plunger TZ-1GV High-temperature Basic Switch, Hinge lever TZ-1GV2 High-temperature Basic Switch, Hinge roller lever TZ-1GV22 High-temperat...
...c switch, Rated carry current 0.1 A, Contact gap 0.25 mm (high-sensitivity), Short hinge roller lever Z-01HW22-B General-purpose Basic switch, Rated carry current 0.1 A, Contact gap 0.25 mm (...
..., 5 A at 250 VAC/ 4 A at 30 VDC, VCTF oil-resistant cable, 3 m D4C-1220 Enclosed Switch, Roller lever, 5 A at 250 VAC/ 4 A at 30 VDC, VCTF oil-resistant cable, 3 m D4C-1220-P Enclosed Switch,...
...ntact welding or other cause. The following diagram shows an example using a rotating shaft and lever. Note 1: The lever cannot be mounted backwards because the protrusion and notch ...
...ctors Non-lighted (Color: Only Black is Available) Sealing IP65 (oil-resistant) Appearance Long lever Notches Reset method Model 2 notches Manual A22S-C2M Automatic A22S-C2A 3 notches Manual ...
...atures Lineup Specifications Dimensions Catalog last update: November 6, 2012 (Unit: mm) Roller lever (Metal lever, resin roller) D4F-[]20-[]R Roller plunger (Metal roller) D4F-[]02-...
https://www.ia.omron.com/products/family/1327/dimension.html