| Site Search | Product Search | IA Global Search |
...its (10 to 15 bits) of CIO 200 to unused (always 0). 20300 20301 20302 20002 Resolution is 720, so 152 is subtracted. No subtraction would be necessary for resolution of 256 or 1,024. If reso...
https://www.fa.omron.co.jp/data_pdf/cat/e6c3-a_ds_e_8_4_csm494.pdf
...tween cables. • Do not lay the cables in parallel with high-voltage lines or power lines. Doing so may result in damage or malfunction due to induction interference. Connection Spurious pul...
https://www.fa.omron.co.jp/data_pdf/cat/e6j-c_ds_e_4_3_csm674.pdf
...ustrial waste. Do not use the Sensor in water, rain, or outdoors. Process the unwired terminals so as not to contact other wiring or devices. Connect the Sensor Head correctly. Otherwise, it ...
https://www.fa.omron.co.jp/data_pdf/cat/e9nc-aa_va_e474-e1_2_2_csm1065027.pdf
... Do not forcibly bend or pull the cables. Do not put a heavy object on them or heat them. Doing so may damage the cables, resulting in a fire. Do not disassemble or alter the unit. There is a...
https://www.fa.omron.co.jp/data_pdf/cat/e9nc-t_e434-e1_10_4_csm1012458.pdf
... sensing object presses the actuator, the light path between the emitter and receiver is broken so that the receiver no longer receives light. (2) Stability Checking Function The light intens...
https://www.fa.omron.co.jp/data_pdf/cat/ee-sa701_801_ds_e_4_3_csm662.pdf
...website. Features Mount Using M2 or M3 Screws The EE-SX95 can be mounted using M2 or M3 screws, so it can easily replace an existing Sensor mounted with M2 screws. Installation with M2 screws...
https://www.fa.omron.co.jp/data_pdf/cat/ee-sx95_e435-e1_3_6_csm1012815.pdf
...Display Two Outputs: Light-ON and Dark-ON All models provide both a light-ON and dark-ON output so that the output can be switched according to the application simply by changing the wiring. ...
https://www.fa.omron.co.jp/data_pdf/cat/ee-sx97_ds_e_1_4_csm2587.pdf
... be less than 10 m. z Installation The photomicrosensor is built into the device being used and so is not equipped to deal with interference from an external light source. When using the sens...
https://www.fa.omron.co.jp/data_pdf/cat/ee-sy671_672_ds_e_6_4_csm486.pdf
...he output status is displayed (outputs 1, 2, 3, and 4). Note: Normally keep this pin set to OFF so that the operation status can be checked. ON: G3ZA Multi-channel Power Controller in operati...
https://www.fa.omron.co.jp/data_pdf/cat/ej1_ds_e_12_5_csm222.pdf
...he output status is displayed (outputs 1, 2, 3, and 4). Note: Normally keep this pin set to OFF so that the operation status can be checked. 7 ON: G3ZA Multi-channel Power Controller in opera...
https://www.fa.omron.co.jp/data_pdf/cat/ej1_h236-e1_4_1_csm1121137.pdf
... automatically across the entire fleet. Enterprise Manager can connect to your MES, ERP and WMS so that jobs can be propagated automatically to the fleet in real time. JOBS JOB 1 JOB 1 JOB 2 ...
https://www.fa.omron.co.jp/data_pdf/cat/enterprisemanager_i834-e-01.pdf
...hile the button on the back is pressed when power is ON. Adjust the position and mounting angle so that the laser pointer beam hits a point 15 mm above the center of the object. (The laser po...
https://www.fa.omron.co.jp/data_pdf/cat/es1-n_h227-e1_4_4_csm1059198.pdf
...the warm-up time as three seconds or more. 6. Ensure sufficient space around the main unit case so that the air vent is not covered. 7. Wire the terminals correctly after confirming the signa...
https://www.fa.omron.co.jp/data_pdf/cat/es2-hb-n_es2-thb-n_h230-e1_2_1_csm1062563.pdf
... moisture, oil, and dust from the surface to which the Sticker is to be attached. Failure to do so may result in insufficient adhesion, and the Sticker may peel away from the surface. 2. When...
https://www.fa.omron.co.jp/data_pdf/cat/f03-15_ds_e_2_2_csm527.pdf
... moisture, oil, and dust from the surface to which the Sticker is to be attached. Failure to do so may result in insufficient adhesion, and the Sticker may peel away from the surface. 2. When...
https://www.fa.omron.co.jp/data_pdf/cat/f03-16pe_ds_e_1_9_csm525.pdf
...3K-@@-D(Black) 2. Do not connect the Conversion Cable for the following purposes. Failure to do so may result in failure. 1. Connecting with the F39-SGIT-IL3, F39-GCNY2, F39-GCNY3 or F39-GCN5...
https://www.fa.omron.co.jp/data_pdf/cat/f3sg-sr_pg_f117-e1_1_9_csm1120108.pdf
...Bracket ) F39-LSGF ・Two b r a c ke t s p e r s e t Suitable for mounting on an aluminum profile so that its center is aligned with the center of beams. Brackets that allow beam adjustment af...
https://www.fa.omron.co.jp/data_pdf/cat/f3sg-sr_pg_f118-e1_1_6_csm1120109.pdf
...sized brackets when performing side mounting 2 for an emitter, with standard mounting brackets, so 2 for a receiver, that total of 4 per set they do not protrude from the detection surface. F...
https://www.fa.omron.co.jp/data_pdf/cat/f3sj_f074-e1_27_11_csm1816.pdf
...ious injury may possibly occur due to loss of required safety functions. Wire F3SP-B1P properly so that supply voltages or voltages for loads do NOT touch the safety inputs accidentally or un...
https://www.fa.omron.co.jp/data_pdf/cat/f3sp-b1p_ds_e_5_1_csm1067236.pdf
...sh simultaneously.) OFF ON Elevator-like lighting (Two adjacent indicators simultaneously light so that lighting moves up and down.) ON ON Accordion-like lighting (Some or all indicators simu...
https://www.fa.omron.co.jp/data_pdf/cat/f3w-d_ds_e_3_5_csm1365.pdf