| Site Search | Product Search | IA Global Search |
...utomation absolute Definition The appropriate product category Rotary Encoders A type of rotary encoder that outputs an absolute position (i.e., the current angle) instead of a relative angle...
...ppropriate product category Rotary Encoders The torque needed to rotate the shaft of the Rotary Encoder at startup. The torque during normal rotation is normally lower than the starting torqu...
...ders A code in which only one bit changes when an address changes. The code plate of the Rotary Encoder uses gray code....
...ervo mount Definition The appropriate product category Rotary Encoders A method of mounting the Encoder in which a Servo Mounting Bracket is used to clamp down the flange of the ...
...ion The appropriate product category Rotary Encoders The output signal count for an Incremental Encoder. There are 1-phase models (phase A), 2-phase models (phase A and phase B), and 3-phase ...
...ulti-turn absolute Definition The appropriate product category Rotary Encoders A type of rotary encoder that provides information on the accumulated position for more than one rotation (i.e.,...
... disk Definition The appropriate product category Rotary Encoders The rotating slit disk in the Encoder is made of metal for higher shock tolerance than glass. Due to slit machining limitatio...
...ppropriate product category Rotary Encoders The torque needed to rotate the shaft of the Rotary Encoder at startup. The torque during normal rotation is normally lower than the starting torqu...
... product category Rotary Encoders The calculated speed for the maximum signal frequency that an Encoder can respond to....
...d from when the Direction Discrimination Unit determines the rotational direction of the Rotary Encoder until an output is made....
...blems from the rotational position where the main power supply fails for an Absolute Multi-turn Encoder. When there is a power failure, multi-turn detection is not performed and the data befo...
...igned to the drive mechanism in an external Servo Drive or the sensing mechanism in an external Encoder Input Slave Unit. Axes Group A functional unit that groups together axes within the Mot...
https://www.ia.omron.com/support/guide/454/explanation_of_terms.html
...Position Interface Unit Position Interface Unit List Position Interface Units for pulse output, encoder input, and SSI input. There are 3 products of Position Interface Unit. NX-series Increm...
...Position Interface Unit Position Interface Unit List Position Interface Units for pulse output, encoder input, and SSI input. There are 3 products of Position Interface Unit. NX-series Increm...
...ted • Digital quadrature encoders, serial encoders, and sinusoidal encoders can be connected as encoder input • 16 digital inputs and 16 digital outputs are built in 更新日期 2019年7月1日 FA...
...ombined with the flexibility of Power PMAC Controller and the ability to interface with various encoder feedback devices, allows the support of the following types of Motors: • AC/DC synchron...
... control using a speed sensor. This method detects the rotation of a motor using a detector (an encoder pulse generator) mounted on the motor and uses vector operation to accurately calculate...
...s Related Contents Cam Positioners Products Primary Contents Cam Positioner Resolver Absolute Encoder Cam Positioner Cam Program Data containing the ON and OFF angles for the cam output tha...
https://www.ia.omron.com/support/guide/12/explanation_of_terms.html
...ect to a Controller with an Analog Output Problem: Noise is superimposed on the feedback pulse (encoder signal), so the Controller takes the noise as a feedback pulse. Countermeasures: Shield...
...ures High-speed Pulses at 50 kHz. Provides high-speed pulse measurements up to 50 kHz of rotary encoder or ON/OFF pulse signals and can perform rotating measurement of high-speed rotating obj...
https://www.ia.omron.com/products/family/1538/application.html