Primary Contents

IAグローバル検索結果

国/地域選択

IAグローバル検索
結果 3761 - 378025804
NYB Industrial PC Platform NY-series Industrial Bo...

...32, 64 or 96 GB 8, 16, 32, 64 GB Memory type DDR4 (ECC is available) DDR4 Package Memory Format SO-DIMM Serial Presence Detect (SPD) Speed grade 3200 MT/s CAS latency CL17 Trusted platform mo...

https://www.omron.com.au/products/family/3631/specification.html

NYP Industrial PC Platform NY-series Industrial Pa...

...ion minimal 10yr) Memory Memory size *1 8, 16, 32, 64 GB Memory type DDR4 Package Memory Format SO-DIMM Serial Presence Detect (SPD) Speed grade 3200 MT/s CAS latency CL17 Trusted platform mo...

https://www.omron.com.au/products/family/3633/specification.html

NX1P2 NX-series NX1P2 CPU Units/Specifications | O...

...ally, turn OFF all of the pins. C SD Memory Card power supply switch Turns OFF the power supply so that you can remove the SD Memory Card. D DIN Track mounting hook These hooks are used to mo...

https://www.omron.com.au/products/family/3650/specification.html

S8FS-G Switch Mode Power Supply (15/30/50/100/150/...

...cteristics of fuses and the operating characteristics of breakers and select fuses and breakers so that external fuses will not burn out or breakers will not operate due to inrush current. Ri...

https://www.omron.com.au/products/family/3656/specification.html

E5CD / E5CD-B Digital Temperature Controller (48 x...

...ection. (Main-tain the specified mounting space between Controllers.) • To mount the Controller so that it is waterproof, insert the water-proof packing onto the Controller. • When two or mor...

https://www.omron.com.au/products/family/3668/dimension.html

E5ED / E5ED-B Digital Temperature Controller (48 x...

...irection. (Maintain the specified mounting space between Controllers.) •To mount the Controller so that it is waterproof, insert the waterproof packing onto the Controller. •When two or more ...

https://www.omron.com.au/products/family/3669/dimension.html

E5CD-800 Digital Temperature Controller (Simple Ty...

...ection. (Main-tain the specified mounting space between Controllers.) • To mount the Controller so that it is waterproof, insert the waterproof packing onto the Controller. • When two or more...

https://www.omron.com.au/products/family/3671/dimension.html

E5ED-800 Digital Temperature Controller (Simple Ty...

...rection. (Maintain the specified mounting space between Controllers.) • To mount the Controller so that it is waterproof, insert the waterproof packing onto the Controller. • When two or more...

https://www.omron.com.au/products/family/3672/dimension.html

K6CM Motor Condition Monitoring Device/Specificati...

...chment is used. *6. Even if the motor is not moving, the value of velocity may appear slightly, so that the measurement value is fixed      at 0.00 mm/s until the value reaches 0.90 mm/s or h...

https://www.omron.com.au/products/family/3686/specification.html

S8VK-X Switch Mode Power Supply (60/120/240/480-W ...

...ning. If the input is connected to a UPS, do not connect a UPS with a square-wave output. Doing so will cause the internal temperature of the product to increase, possibly causing smoking or ...

https://www.omron.com.au/products/family/3687/specification.html

S8V-NF Noise Filter (Single-phase 250 V 3 A / 6 A ...

...2 *1. If the input is connected to a UPS, do not connect a UPS with a square-wave output. Doing so will cause the internal        temperature of the product to increase, possibly causing smok...

https://www.omron.com.au/products/family/3688/specification.html

E3NX-MA Smart Fiber Amplifier Units/Specifications...

...32-LD11 2M 820 330 250 74 E32-LD11R 2M 790 310 240 71 *1. The fiber length is 2 m on each side, so the sensing distance is given as 4,000 mm. Cylindrical Models Sensing method Size Sensing di...

https://www.omron.com.au/products/family/3694/specification.html

NX-TC NX-series Temperature Control Unit/Specifica...

...tal Filter This function sets the time constant applied to the first-order lag operation filter so that the noise components mixed with the measured value are eliminated. All models Measuring...

https://www.omron.com.au/products/family/3699/specification.html

E8FC IoT Flow Sensors/Lineup | OMRON Industrial Au...

...e theme on both the piping side and the sensor mounting side.    Because the sensor is designed so that the measurement area is in the center of the piping, correct measurement    may not be ...

https://www.omron.com.au/products/family/3720/lineup.html

F3SG-SR / PG Series Safety Light Curtain/Safety Mu...

.... Z405). Note: 2. Do not connect the Conversion Cable for the following purposes. Failure to do so may result in failure.              1. Connecting with the F39-SGIT-IL3, F39-GCNY2, F39-GCNY...

https://www.omron.com.au/products/family/3736/lineup.html

S8VK-WA Switch Mode Power Supply (240/480/960/2000...

...If the input is connected to a UPS, do not       connect a UPS with a square-wave output. Doing so will cause the internal temperature of the product to increase,       possibly causing smoki...

https://www.omron.com.au/products/family/3753/specification.html

R88M-1A[] / R88D-1SAN[]-ECT AC Servo System 1S-ser...

... test (insulation resistance measurement)              on a Servo Drive.              Not doing so may result in the Servo Drive failure.              Do not perform a dielectric strength tes...

https://www.omron.com.au/products/family/3776/specification.html

S8V-CP DC Electronic Circuit Protector (24 VDC 4 O...

...mA max. Note: 1. Alarm signal output is not equipped with an internal current limiting circuit, so be sure that the current flowing to the alarm signal output terminals does not exceed 50 mA....

https://www.omron.com.au/products/family/3780/specification.html

D4GS-N Slim Safety Door Switch/Dimensions | OMRON ...

...4GS-NK4 Note 1. When determining the operation key insertion radius, adjust the adjusting screw so that the tip of the operation              key is positioned to the center of the key insert...

https://www.omron.com.au/products/family/379/dimension.html

H7CC-A Digital Counter/Dimensions | OMRON Industri...

...s should be 1 to 5 mm. 2. To allow easier operation, it is recommended that Adapters be mounted so that the gap between sides with hooks is at least 15 mm (i.e., with the panel cutouts separa...

https://www.omron.com.au/products/family/3809/dimension.html

結果 3761 - 378025804

国/地域選択

Related Contents