| IAグローバル検索 |
...xel Measurement Feature In the ROI processing, one of the following measurement features can be se- lected for one model. •Binary feature •Gray-scale feature •Binary incremental correlation v...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/z109-02a_f350.pdf
...in which the patterns of the alphanumeric characters to be read were registered. Refer to 4-9-2 Se- lecting the Dictionary. DUMMY(P27) Steady Character Reading Section 3-2 35 15. Select read ...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/z111-e1-01_f350-u004e.PDF
...er application programs. •Do not open the MMI Unit’s Memory Card cover from the time“S.Scene”is se- lected until you return to the menu bar. When an F350-C41E IMP Unit is used, a Memory Card ...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/z112-e1-01_f350-u005e.PDF
...er application programs. •Do not open the MMI Unit’s memory card cover from the time“S.Scene”is se- lected until you return to the menu bar. When an F350-C41E IMP Unit is used, a memory card ...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/z113-e1-01_f350-u006e.PDF
...er application programs. •Do not open the MMI Unit’s memory card cover from the time“S.Scene”is se- lected until you return to the menu bar. When an F350-C41E IMP Unit is used, a memory card ...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/z114-e1-01_f350-u007e.PDF
...e select“2-model posi- tioning”by using two model marks in different positions. Refer to 4-12-1 Se- lecting the Position Compensation Mode. P5 7. Register the position compensation model. Reg...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/z115-e1-01_f350-u008e.PDF
... 18 2-2 Sensors There are four kinds of Sensors that can be used with the Intelligent Flag III. Se- lect a Sensor to suit the application. 2-2-1 Specifications Item V600-HS51 V600-HS61 V600-H...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/z129-e1-02_v600-ham42-drt.pdf
... be used to com- municate with exter- nal devices. →p. 21, 37 Two communications methods can be se- lected for RS-232C: Normal and Host link →p. 140 Personal computer Specifications Reading c...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/z136-e1-01_v530-r150.pdf
...r the correlation with themodel and the coordinates where themodel is found. Model registration Se Ca Correlation :79 [80: 100] Position X : 180 [ 0.000 : 511.000] Position Y : 250 [ 0.000 : ...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/z142-e3-1_f150.pdf
...t STEPas the image storage method and select memory image 35. (Refer to page 22.) 4-1-3Changing Se tting Details Adding Regions Yes Back No This scene has been set already. Clear all settings...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/z145-e1-02_f160.pdf
.......................................................... 5-19 5-8-5 Operation Condition Setting (SE)...............................................................................................
https://www.fa.omron.com.cn/data_pdf/closed/mnu/z148-e1-06_v670-cd1d-v1_h11_h51(q)_d13f0_(h).pdf
...Display Bits (D)) Section 3-12 ware version 1.10 or later. For details on the CPU Unit version, se- lect Other/System information. (Refer to page 94.) ZEN Support Software of Ver. 2.00 or lat...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/z183-e1-01a_zen.pdf
.... Error in communi- cation between IDRWH and ID tag 70 Communications error•A fault such as noi se interference has occurred during data trans- action with ID tag, and the communication opera...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/z213-e1-01b_v700-l11_hmd1___d23p41-1.pdf
...h outputs that were connected will be reconnected according to the pattern set with the startup se- quence and all of the new parameters will be effective at this time. Immediately afterward,...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/z241-e1-03_s8m.pdf
...RESET MEAS/MGNIFY ↑↓50.000mm ←→123LINE SET MEAS/MGNIFY ↑↓10.000mm ←→450LINE SET MEAS/MGNIFY ←→↑↑SE MEAS/MGNIFY MAGNIFY PROFILE YES NO Measurement Settings 69 ZG User’s Manual 3 FUNCTION SETTI...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/z250-e1-02_zg.pdf
...Checking SystemConfiguration 21 Reference ●Fo r detail s o n connecto r specifications , etc. , se e th e "Operator' s Manua l (Setup) " o f eac h model. Descriptio n o f Model-specifi c Func...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/z290-e1-05_fz3.pdf
...tc h th e image. Reference : Camer a Switchin g (p.44) Camer a Setting s (Camer a Imag e Input) Se t th e followin g photographin g condition s fo r eac h camera. ●Reference : Camer a Setting...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/z291-e1-05_fz3.pdf
...Dis k o r RAMDis k a s files. Whe n "Sav e t o memor y + file " in "Destination " is selected , se t th e destinatio n an d fil e names. Settin g item Settin g value [Factor y default] Descri...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/z318-e1-02b_fz4.pdf
...tc h th e image. Reference : Camer a Switchin g (p.50) Camer a Setting s (Camer a Imag e Input) Se t th e followin g photographin g condition s fo r eac h camera. ●Reference : Camer a Setting...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/z319-e1-02_fz4.pdf
...ess Gate signal output (GATE) Selected task output (BINARY_OU T1/2) Selected task input (BINARY_SE L1/2) DC input system Input voltage: 24 VDC±10 % (21.6 to 26.4 VDC) Input current: 7 mA Typ....
https://www.fa.omron.com.cn/data_pdf/closed/mnu/z322-e1-05_zw-c1_t.pdf