| IAグローバル検索 |
... required to connect the Servo Relay Unit’s communications port and the Programmable Controller Se- rial Communications Unit or Board. The communications cable length can be 1 or 2 meters lon...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/i533-e1-04_r7m-a_r7d-ap.pdf
... changements de température extrêmes ・Les emplacements oùdu givre ou de la condensation peuvent se former ・Les emplacements sujetsàdes chocs ouàdes vibrations excessifs 2) Ne pas utiliser l...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/k3te_inst-2381913-3d.pdf
... changements de température extrêmes ・Les emplacements oùdu givre ou de la condensation peuvent se former ・Les emplacements sujetsàdes chocs ouàdes vibrations excessifs 2) Ne pas utiliser l...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/k3tf_inst-2381914-1f.pdf
...s internes. Serrer les vis des bornes au couple de réglage prescrit (0,69-0,88 N·m). Si les vis se desserrent, il existe une certaine possibilitéd’incendie ou de dysfonctionnement. Ne pas int...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/km20-a__inst-7452283-6c.pdf
...OPERATION MANUAL Cat. No. M071-E1-02 WD30-ME/-SE/-ME01/-SE01 DeviceNet Wireless Units Copyrights and Trademarks DeviceNet is a registered trademark of the OpenDeviceNet Vendor Association (OD...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/m071-e1-02_wd30-me_-se.pdf
...3NX stops measurement in setting mode. Some menus cannot be set ac- cording to the Output Board se- lected. If the input range is changed, all the other parameters are set to default values. ...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/n090-e1-01b_k3nx.pdf
...K3NX stops measurement in settingmode. Some menus cannot be set ac- cording to the Output Board se- lected. If the input range is changed, all the other parameters are set to default values. ...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/n090-e3-1_k3nx.pdf
...e next parameter. The input value will be validated automatically if no change is made for five se- conds. The bps baud rate setting will be displayed again. Set Value LED Display Model Basic...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/n093-e1-01a_k3nr.pdf
...K3NV stops measurement in settingmode. Some menus cannot be set ac- cording to the Output Board se- lected. If the input range is changed, all the other parameters are set to default values. ...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/n91-e3-1_k3nv.pdf
...following table. Note (1) The external pulse output from the port is disabled when this mode is se- lected. (2) A pulse output port that is being used as a pulse counter timer cannot be used ...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/o010-e1-01_fqm1-cm001_mmp21_mma21.pdf
...: mantissa 23 The mantissa portion of binary floating-point data fits the formal 2.0 > 1.f≥1.0. se f 31 30 23 22 0 Sign Exponent Mantissa −1.175494×10–38 1.175494×10–38 –∞+–3.402823×1038 3.40...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/o011-e1-01_fqm1-cm001_mmp21_mma21.pdf
...following table. Note (1) The external pulse output from the port is disabled when this mode is se- lected. (2) A pulse output port that is being used as a pulse counter timer cannot be used ...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/o012-e1-03_fqm1-com_mm.pdf
...: mantissa 23 The mantissa portion of binary floating-point data fits the formal 2.0 > 1.f≥1.0. se f 31 30 23 22 0 Sign Exponent Mantissa −1.175494×10–38 1.175494×10–38 –∞+–3.402823×1038 3.40...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/o013-e1-03_fqm1-com_mm.pdf
...代碍(通常力二遊観)。 ---------------------[End of Page 4629]--------------------- 栓姶和 checks㎜ 吋紳肺沖 c1㏄kp汕se 日守神月永}中位 c1㏄kpulsebit 公共数据 commondata 通信亀鋭 commUnicationc...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/oez-zdp00101a_cqm1h_discon.pdf
...fore using the System. •Be sure that the DC Power Supply Unit exclusively designed for the V700 Se- ries is used and is not connected to any other device. •Be sure that the power supply volta...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/q113-e1-07_v700-cd_d-v3.pdf
...errez les vis des terminaux avec un couple de torsion de 6.6 in-lb (0.74 N•m). Un incendie peut se déclarer si des vis sont desserrées. •Ne pas toucher les terminaux dans les 1 minutes suivan...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/s82k_inst-0646113-6d.pdf
... puissentêtre remplies durant le fonctionnement en parallèle. ■Conformitéavec les directives CE Se reporter au catalogue et au manuel de fonctionnement pour plus de détails au sujet des condi...
... puissentêtre remplies durant le fonctionnement en parallèle. ■Conformitéavec les directives UE Se reporter au catalogue et au manuel de fonctionnement pour plus de détails au sujet des condi...
...excès de courant de plus de 20 secondes, les composants internes du bloc d'alimentation peuvent se détériorer ou s'abîmer. ■Protection contre les surtensions Ce modèle est automatiquement pro...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/s8ts_inst-0697228-9f.pdf
...excès de courant de plus de 20 secondes, les composants internes du bloc d'alimentation peuvent se détériorer ou s'abîmer. 2. Autrement, les pièces internes pourraientêtre détériorées ou endo...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/s8ts_inst-2149191-2d.pdf