| IAグローバル検索 |
...t de–25à+65°C et l’humiditérelative de 25à90%. 2.Leséléments internes peuvent occasionnellement se détériorer ouêtre brisés suiteàune mauvaise dissipation de chaleur liée au sens du montage. ...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/s8vm(15,30,50,100,150w)_inst-1618626-5f.pdf
...die Einhaltung der EMV- Richtlinien wird auf den Katalog und die Bedienungsanleitung verwiesen. Se reporter au catalogue et au manuel de fonctionnement pour plus de détails au sujet des condi...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/s8vm(15_30_50_100_150w)_inst-1618627-3f.pdf
...t ouvertes. Réalisez les connexions correctes comme spécifié. ■Conformitéavec les directives UE Se reporter au catalogue et au manuel de fonctionnement pour plus de détails au sujet des condi...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/s8vm(300_600_1500w)_inst-1618744-0e.pdf
...t de–25à+65°C et l’humiditérelative de 25à90%. 2.Leséléments internes peuvent occasionnellement se détériorer ouêtre brisés suiteàune mauvaise dissipation de chaleur liée au sens du montage. ...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/s8vm(300w,600w,1500w)_inst-1618743-1e.pdf
...roducts whose vis- ible emission does not exceed Class I limits for emission durations of 1,000 se- conds or less and are not intended for viewing. Class 2 lasers are divided into two subclas...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/scha-716a-24_eng_z4lc.pdf
...HIGH threshold: Improper product Note The discrimination outputs can be changed. Refer to 4-2-2 Se- lecting the Discrimination Outputs for details (p. 39). There are three methods to set thre...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/scha-719a-26_eng_z4lb_v2.pdf
...形SEモータ・リレー取扱説明書 5497312-2C ©OMRON Corporation 2015 All Rights Reserved. オムロン製品をお買いあげいただきありがとうございます。 ご希望どおりの製品かお確かめいただき、この取扱説明...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/se_inst-5497312-2c.pdf
...URE O INSTALLAZIONI DI TIPO INDUSTRIALE. NONÈDESTINATO ALL'USO DIRETTO DA PARTE DEI CONSUMATORI SE NON APPOSITAMENTE PROGETTATO ALLO SCOPO. I fornitori di queste attrezzature, apparecchiature...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/swal-cn5-706f_mx-z2000h_discon.pdf
...ller mode’s system settings. 2. Either PT memory switches or CompoBus/D setting switches can be se- lected from the memory switch initialization menu. Select PT memory switches to initialize ...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/v066-01_nt-drt21.pdf
.... For details on methods for connecting the host, refer to Section 4 Connecting the Host to the Se- rial Port or Section 5 Connecting to Host via Ethernet or Controller Link. 3-1Installing th...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/v072-02_ns12-ts_ns10-tv_ns7-sv.pdf
... & EXIT Select“Page”. If the host link is not select- ed, press the“Comm. Type”touch switch and se- lect“Host link”. Automatic Reset Baud Rate No 9600bps (2/2) Quit [ MEMORY SW MENU ] Page WR...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/v091-e1-01_nt20.pdf
...at the PT has a lot number that supports USB transmission. The system program version of the NS-se- ries PT must also support USB transmission. For details, refer to 3-3-2 Connecting via USB ...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/v099-e1-12_ns-cxdc1-v3.pdf
...r at the PLC to 0. 1,2,3... 1. Under Network Type in the Change PLC Dialog Box, select“NV-Thru (Se- rial Port)”for the network type. Computer running NV-Designer CX-Programmer Ladder diagrams...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/v103-e1-10_nv3w_nv4w_nv3q_setup.pdf
...r Menu to open the NV Configuration Dialog Box. If multiple project files are already open, the Se- lect File Dialog Box will be displayed. Select a project file to set up. 2. Set the require...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/v104-e1-07_nv3w_nv4w_nv3q.pdf
...THEOMRONPROOUCTISPROPEFIILYRA[正D州0 1NSTALLEDFOR¶HE‖ト『ENDEOUSEW:THINTHEOVERALL EQUZPM日N「ORSYSTEM Se●elgoPr◎du巴tca栖10gforV㎞自rW日ndUmitatlonoiUahllltSt. ■EUIROPE OMRONa瓢)P日E.「V,Sens...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/v700-h31_inst-1607756-3b.pdf
...- ler Link Network. Note 1. The Controller Link Support Software cannot be connected to a CS/CJ-se- ries PLC. It is possible to monitor and set a Controller Link Unit on a CS/ CJ-series via t...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/w309-e1-12_c_1w_c200hw_cvm1_cqm1h-clk_cs1w-rpt.pdf
...rature Sensor Unit Thermocouple inputs 3 Units max. (See note.) 2 inputs (K, J) --- CPM1A-TS001 Se so U pu s 1 Unit max. 4 inputs (K, J) CPM1A-TS002 Platinum resistance thermometer 3 Units ma...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/w317-e1-11_cpm1a.pdf
...ing to the input type and input range as shown in the following table to the input terminal (as se- 161 GT1-TS04T and GT1-TS04P Temperature Input Units Section 5-3 lected in step 7) on the Te...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/w348-e1-08_drt1-com_gt1.pdf
...rature Sensor Unit Thermocouple inputs 3 Units max. (See note.) 2 inputs (K, J) --- CPM1A-TS001 Se so U pu s 1 Unit max. 4 inputs (K, J) CPM1A-TS002 Platinum resistance thermometer 3 Units ma...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/w352-e1-07_cpm2a.pdf
...pose external devices with a serial port (e.g., RS-232C). Note This mode is supported only by a Se- rial Communications Board. No No Yes Clock Some Memory Cassette are equipped with a clock. ...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/w363-e1-07_cqm1h.pdf