| IAグローバル検索 |
...ting Electric Shock The ground is needed to prevent electric shock in case of electric leakage. 61F-G[]N Improved Design for a More Lightweight Construction and Reduced Standby Power Consumpt...
...be performed by leaving the E2 electrode unused and making no connections to terminals 6 and 7. 61F-G[]N Improved Design for a More Lightweight Construction and Reduced Standby Power Consumpt...
...ation where there is a noise source such as an inverter, because it may result in malfunctions. 61F-G[]N Improved Design for a More Lightweight Construction and Reduced Standby Power Consumpt...
...re is no pressure applied. In other words, the operating pressure must be atmospheric pressure. 61F-G[]N Improved Design for a More Lightweight Construction and Reduced Standby Power Consumpt...
...sible. A voltmeter able to read a value of several volts with as high an impedance as possible. 61F-G[]N Improved Design for a More Lightweight Construction and Reduced Standby Power Consumpt...
...ll also repeatedly turn ON and OFF, so the lifetime of the contacts will be shorter than usual. 61F-G Example Applicable Models 61F-G/61F-GH/61F-GD/61F-GR/61F-GL 2km/61F-GL 4km/...
...o. FAQ03310 Related Contents Primary Contents Question Can you explain the wiring for combining 61F-G Floatless Level Controllers with an upper-limit float switch and a lower-limit float swit...
...erate even with low-conductivity liquids, thus raising the sensitivity of the Level Controller. 61F-G[]N Improved Design for a More Lightweight Construction and Reduced Standby Power Consumpt...
...than necessary may result in faulty resetting due to condensation forming in Electrode Holders. 61F-G[]N Improved Design for a More Lightweight Construction and Reduced Standby Power Consumpt...
...provide any special brackets for this purpose. Use a commercially available bracket if desired. 61F-G[]N Improved Design for a More Lightweight Construction and Reduced Standby Power Consumpt...
...ormally open terminal 4. Lamp terminal (If DC polarity is required, it is indicated by + and -) 61F-G[]N Improved Design for a More Lightweight Construction and Reduced Standby Power Consumpt...
...l resistor. Pushbutton Switches "A16" (M16), "A22" (M22), "A3P" (M2P), "A3K" (M2K), "A3S" (M2S) 61F-G[]N Improved Design for a More Lightweight Construction and Reduced Standby Power Consumpt...
... Answer The Socket Unit is the unit that opens and closes the electrical circuit. Socket Unit 61F-G[]N Improved Design for a More Lightweight Construction and Reduced Standby Power Consumpt...
...nfirmed using oils and cutting oils stipulated by OMRON (equivalent to previous JEM standards). 61F-G[]N Improved Design for a More Lightweight Construction and Reduced Standby Power Consumpt...
...base plate of the Operating Unit. It is built in and cannot be removed from the Operating Unit. 61F-G[]N Improved Design for a More Lightweight Construction and Reduced Standby Power Consumpt...
...3600T Sealing Caps (for projection models), or A22Z-3600G Sealing Caps (for full-guard models). 61F-G[]N Improved Design for a More Lightweight Construction and Reduced Standby Power Consumpt...
...e a switch has been operated and the button released, the switch returns to its initial status. 61F-G[]N Improved Design for a More Lightweight Construction and Reduced Standby Power Consumpt...
...anical lock mechanism. The pull action releases the lock and returns the contact to OFF status. 61F-G[]N Improved Design for a More Lightweight Construction and Reduced Standby Power Consumpt...
...separated and so it is necessary to connect them. The terminal layout of the A16 is as follows. 61F-G[]N Improved Design for a More Lightweight Construction and Reduced Standby Power Consumpt...
..., OMRON does not engrave or print Legend Plates. Please find a printing company to do the work. 61F-G[]N Improved Design for a More Lightweight Construction and Reduced Standby Power Consumpt...