| IAグローバル検索 |
... the Counter cannot be reset. To enable key operations, set the Key Protect Switch to OFF. K3HB-X A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current ...
...ng currents and voltages can be switched. H7BR: 5 V, 2 mA H7HP: 5 V, 2 mA H7EC: 3 V, 20 μA K3HB-X A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current ...
...ignal will not be detected and the input will remain ON, resulting in abnormal operations. K3HB-X A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current ...
...n Can the batteries of the H7E[]-N be replaced? Answer Yes. Applicable Battery: Y92S-36. K3HB-X A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current ...
...of times that EEPROM can be written (i.e., the number of overwrites), however, is limited. K3HB-X A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current ...
...t use no-voltage input? Answer Recommended model: OMRON Solid-state Relay the G3TA-IA/ID K3HB-X A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current ...
...o OFF time. (The Counter's maximum counting speed is specified at an ON/OFF ratio of 1:1.) K3HB-X A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current ...
...the batch output and batch count display. Applicable Models: H7BR-B, H7CX-A4W[], H7CX-AW[] K3HB-X A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current ...
...blem persists for more than a few minutes, consult with your nearest OMRON representative. K3HB-X A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current ...
...Note: The inrush current time is measured in the wave range shown in the following figure. K3HB-X A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current ...
...What Preset Counter models are available? Answer Refer to the following selection guide. K3HB-X A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current ...
...er used to operate a control output when the count value reaches a preset numerical value. K3HB-X A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current ...
...r Total Counters display the count value only and are not provided with control outputs. K3HB-X A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current ...
...N is cut, so choose a DC voltage input model. 2.Be careful when using the power-OFF reset. K3HB-X A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current ...
...ameters can be set using DIP switches or a similar method, with no power supply necessary. K3HB-X A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current ...
...2 PV = 6. The dual count value after subtraction is CP1 PV - CP2 PV, therefore 11 - 6 = 5. K3HB-X A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current ...
... function is activated and the display becomes zero. Applicable models: H7CX-R and H7CX-AW K3HB-X A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current ...
...ice it will not be displayed. Instead, unit labels (-hours/-d-h/-h-m/-h-m-s) are provided. K3HB-X A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current ...
...G3J-205BL For example, G3J-205BL withstands an inrush current of 150 Apeak. Therefore R > 200 V x √2/150 A = 1.9 Ω Considering the circuit current and ON time, insert the protective resistanc...
...ays can be found using the following equation. Heating value P (W) = Output-ON voltage drop (V) x Carry current (A) For example, if a load current of 8 A flows from G3NA-210B Solid-state Rela...