| IAグローバル検索 |
...f Photomicrosensors. Be sure to check the items to find which Photomicrosensors are applicable. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What is the respons...
...出 促銷價 1010 元 E5CC-RX2ABM-802 (原價3800) Push-In數位溫控器-48×48mm AC100~240V 繼電器輸出 RS-485通訊 促銷價 1700 元 E2E-X2E2 2M (原價790) M12; 直流3線式; 隔離型; NPN輸出; 出線型 促銷價 420...
...ray 2 6 11 Shielded Shielded Shielded (GND) 12 Red Red 12 to 24 VDC 13 Black Black 0 V (common) E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions How far should the ...
...d will be applied to the shaft, which may result in damage or extremely shortened service life. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What are the lead w...
...9-C08B 6.8 mm E69-C10B 7.1 mm E69-C68B 6.8 mm E69-C610B 7.1 mm E69-C06M 8.5 mm E69-C10M 10.5 mm E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What are the lead w...
...品性 出線型、直流3線NPN輸出及氟樹脂塗裝型一應俱全 更新日期 2015年8月8日 感測器 近接感測器 圓柱型 E2E NEXT E2E(小徑型) E2E E2EW E2EF E2FM E2EQ NEXT E2EQ E2EZ E2EH E2F E2FQ E2...
...新日期 2015年8月8日 SUS316L本體、IP69K、高溫使用環境、耐洗淨劑- 更新日期 2015年8月8日 感測器 近接感測器 圓柱型 E2E NEXT E2E(小徑型) E2E E2EW E2EF E2FM E2EQ NEXT E2EQ E2EZ E...
...容請參閱特性資料。 *2. 在轉數130rpm下以不銹鋼刷測試的結果 更新日期 2015年8月8日 感測器 近接感測器 圓柱型 E2E NEXT E2E(小徑型) E2E E2EW E2EF E2FM E2EQ NEXT E2EQ E2EZ E2EH E2...
...ne inventory management and save a great deal of inventory space. 更新日期 2025年11月4日 感測器 近接感測器 圓柱型 E2E NEXT E2E(小徑型) E2E E2EW E2EF E2FM E2EQ NEXT E2EQ E2EZ...
...而分離,也不容易發生檢測錯誤 即使工件的位置有差異也不易引發碰撞 長距離穩定檢測技術「溫度距離控制 × IoT」 E2E NEXT 系列利用長距離穩定檢測技術「溫度距離控制」與類比數位複合 IC,來解決將近接感測...
...增長距離型系列。最長檢測距離15mm 亦備有Smartclick接頭中繼型 更新日期 2015年8月8日 感測器 近接感測器 圓柱型 E2E NEXT E2E(小徑型) E2E E2EW E2EF E2FM E2EQ NEXT E2EQ E2EZ E2EH E...
...8月8日 耐化學性優異的全氟樹脂 最長檢測距離10mm 更新日期 2015年8月8日 感測器 近接感測器 圓柱型 E2E NEXT E2E(小徑型) E2E E2EW E2EF E2FM E2EQ NEXT E2EQ E2EZ E2EH E2F E2FQ E2EY ...
...於檢測體的檢測而 不產生誤動作 亦備有Smartclick接頭中繼型 更新日期 2015年8月8日 感測器 近接感測器 圓柱型 E2E NEXT E2E(小徑型) E2E E2EW E2EF E2FM E2EQ NEXT E2EQ E2EZ E2EH E2F ...
...的超群保護構造 防止相互干擾(亦備有不同頻率的機型) 更新日期 2015年8月8日 感測器 近接感測器 圓柱型 E2E NEXT E2E(小徑型) E2E E2EW E2EF E2FM E2EQ NEXT E2EQ E2EZ E2EH E2F E2FQ ...
...屬(鋁、黃銅等)* • 不檢測磁性金屬(鐵、鎳等) *但無法檢測鋁箔 更新日期 2015年8月8日 感測器 近接感測器 圓柱型 E2E NEXT E2E(小徑型) E2E E2EW E2EF E2FM E2EQ NEXT E2EQ E2EZ E...
...c objects, and sensors that utilize magnetic DC fields as Proximity Sensors. PDF Download(30KB) E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions E2EH Proximity Sens...
... E8F2 outside the measurement range. Countermeasure: Use the E8F2 within the measurement range. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions Are Pressure Sensor...
...e (-) port. Use the port as the negative (-) port when it is left open to atmospheric pressure. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions The zero-reset func...
...play.) Not saving the set value: Press and at the same time. (Valid for any set value display.) E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions The zero-reset func...
...E4R Ultrasonic Sensor Amplifier should not be used in an ambient temperature higher than 40 °C. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions Which Sensors can b...