Primary Contents

IAグローバル検索結果

国/地域選択

IAグローバル検索
結果 1841 - 18604543
FAQ01126 for Photomicro Sensors | OMRON Industrial...

... usage restrictions and electrical and optical characteristics indicate the performance limits. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What is the respons...

https://www.ia.omron.com/support/faq/answer/24/faq01126/

FAQ01127 for Photomicro Sensors | OMRON Industrial...

... V CE(sat) )/R L + 0.1 R L > ((5 − 0.1)/(0.212 − 0.1)) = 43.8k Ω ,so R L = Approximately 47 kΩ. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What is the respons...

https://www.ia.omron.com/support/faq/answer/24/faq01127/

FAQ01133 for Photomicro Sensors | OMRON Industrial...

... usage restrictions and electrical and optical characteristics indicate the performance limits. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What is the respons...

https://www.ia.omron.com/support/faq/answer/24/faq01133/

FAQ01138 for Photomicro Sensors | OMRON Industrial...

...t can be applied to the emitter of a phototransistor with the collector at reference potential. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What is the respons...

https://www.ia.omron.com/support/faq/answer/24/faq01138/

FAQ01154 for Photomicro Sensors | OMRON Industrial...

...d models External light interference Susceptibility to ambient light Resistant to ambient light E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What is the respons...

https://www.ia.omron.com/support/faq/answer/24/faq01154/

FAQ01165 for Photomicro Sensors | OMRON Industrial...

... recovery time is calculated as follows. Applicable Products: Built-in Type Photomicro Sensors. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What is the respons...

https://www.ia.omron.com/support/faq/answer/24/faq01165/

FAQ01171 for Photomicro Sensors | OMRON Industrial...

...-1006", "EE-1010", and Robot Cable Connector "EE-1010-R" with the open terminals are available. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What is the respons...

https://www.ia.omron.com/support/faq/answer/24/faq01171/

FAQ01172 for Photomicro Sensors | OMRON Industrial...

...is released. Generally, the operate time (tON) is almost equivalent to the release time (tOFF). E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What is the respons...

https://www.ia.omron.com/support/faq/answer/24/faq01172/

FAQ01174 for Photomicro Sensors | OMRON Industrial...

...d Photomicrosensors for Industrial Equipment that are resistant to external light interference. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What is the respons...

https://www.ia.omron.com/support/faq/answer/24/faq01174/

faq01177

...s a lock mechanism to prevent connectors from disconnecting, but EE-1001 has no lock mechanism. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What is the respons...

https://www.ia.omron.com/support/faq/answer/24/faq01177/

faq01178

...of the cable.) Using EE-1010-R is recommended if the cable is to be connected to a moving part. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What is the respons...

https://www.ia.omron.com/support/faq/answer/24/faq01178/

faq01179

... mechanism to prevent the connector from being disconnected, but EE-1006 has no lock mechanism. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What is the respons...

https://www.ia.omron.com/support/faq/answer/24/faq01179/

FAQ01182 for Photomicro Sensors | OMRON Industrial...

...re should be repeated until a cable is absolutely cut off. Fig.1 Cable Bending Destruction Test E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What is the respons...

https://www.ia.omron.com/support/faq/answer/24/faq01182/

FAQ01184 for Photomicro Sensors | OMRON Industrial...

... EE-SPX741 EE-SPX-W EE-SPX302-W2A EE-SPX304-W2A EE-SPX306-W2A EE-SPX305-W2A EE-SPX303 EE-SPX301 E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What is the respons...

https://www.ia.omron.com/support/faq/answer/24/faq01184/

FAQ02655 for Photomicro Sensors | OMRON Industrial...

...ort-circuit protection circuit for the output. Care must be taken to avoid connection mistakes. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What is the respons...

https://www.ia.omron.com/support/faq/answer/24/faq02655/

faq02661

...nge or deterioration in the illuminating LED over time (even if initial operation was correct). E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What is the respons...

https://www.ia.omron.com/support/faq/answer/24/faq02661/

faq02676

...Sensors: Approx. 0.2 to 0.5 mm (If the sensing object travels parallel to the sensing surface.) E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What is the respons...

https://www.ia.omron.com/support/faq/answer/24/faq02676/

faq02681

... be inserted (as a smoothing circuit) to prevent unstable operation due to the drop in voltage. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What is the respons...

https://www.ia.omron.com/support/faq/answer/24/faq02681/

faq02685

...or output short-circuit protection circuit. Care must be taken to prevent incorrect connection. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What is the respons...

https://www.ia.omron.com/support/faq/answer/24/faq02685/

faq02687

...or connected to the positive terminal, so leave it open or connect it to the positive terminal. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What is the respons...

https://www.ia.omron.com/support/faq/answer/24/faq02687/

結果 1841 - 18604543

国/地域選択

Related Contents