Primary Contents

IAグローバル検索結果

国/地域選択

IAグローバル検索
結果 1861 - 18804543
faq03129

...g at least 2 x 0.8 mm for the EE-SX47/67 Series Dimensions of emitter/receiver slit: 2 x 0.8 mm E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What is the respons...

https://www.ia.omron.com/support/faq/answer/24/faq03129/

faq03460

...electronic circuits) or if EE-SX671 is used near the source of a high-frequency magnetic field. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What is the respons...

https://www.ia.omron.com/support/faq/answer/24/faq03460/

FAQ00937 for Rotary Encoders | OMRON Industrial Au...

...tion? Answer  For the reverse rotation, please wire the Phase A and Phase B outputs reversely. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What are the lead w...

https://www.ia.omron.com/support/faq/answer/34/faq00937/

FAQ00939 for Rotary Encoders | OMRON Industrial Au...

...E6J-C Series of incremental Rotary Encoder? Answer  The main difference points are as follows. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What are the lead w...

https://www.ia.omron.com/support/faq/answer/34/faq00939/

FAQ00941 for Rotary Encoders | OMRON Industrial Au...

...necessary for resolution. e.g. * The Gray code change only 1 bit, the binary code change 5 bit. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What are the lead w...

https://www.ia.omron.com/support/faq/answer/34/faq00941/

FAQ00946 for Rotary Encoders | OMRON Industrial Au...

...ase A and phase Z serial, to take timing with rising or falling of phase A to improve accuracy. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What are the lead w...

https://www.ia.omron.com/support/faq/answer/34/faq00946/

FAQ00948 for Rotary Encoders | OMRON Industrial Au...

...digit of a decimal number is expressed using a binary value. Absolute code table is as follows. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What are the lead w...

https://www.ia.omron.com/support/faq/answer/34/faq00948/

FAQ00951 for Rotary Encoders | OMRON Industrial Au...

...nt of an incremental signal output when the shaft revolves once, or the absolute address count. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What are the lead w...

https://www.ia.omron.com/support/faq/answer/34/faq00951/

FAQ00955 for Rotary Encoders | OMRON Industrial Au...

...g cable distance. They can be connected to open-collector input devices (NPN, PNP). E6C3-CWZ5GH E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What are the lead w...

https://www.ia.omron.com/support/faq/answer/34/faq00955/

FAQ00968 for Rotary Encoders | OMRON Industrial Au...

...21 * Please confirm details with the applicable Date Sheet. Please examine with the above unit. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What are the lead w...

https://www.ia.omron.com/support/faq/answer/34/faq00968/

FAQ00969 for Rotary Encoders | OMRON Industrial Au...

...e wire by twisting two outputs and takes off the noise component. Purchase is possible in 100m. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What are the lead w...

https://www.ia.omron.com/support/faq/answer/34/faq00969/

FAQ00972 for Rotary Encoders | OMRON Industrial Au...

... a rotation by the counter installed internally, multi-turn data is output as an absolute code. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What are the lead w...

https://www.ia.omron.com/support/faq/answer/34/faq00972/

faq00977

... reduce the installation space. E6H-C E6C-NN5CA (Pre-wired Model) E6C-NN5CA-C (Connector Model) E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What are the lead w...

https://www.ia.omron.com/support/faq/answer/34/faq00977/

FAQ00978 for Rotary Encoders | OMRON Industrial Au...

...de and adjust the origin so cut face "D" and phase "Z" origin of other models are not suitable. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What are the lead w...

https://www.ia.omron.com/support/faq/answer/34/faq00978/

FAQ00986 for Rotary Encoders | OMRON Industrial Au...

... and confirm whether coupling is correctly mounted or the transmission system doesn't run idle. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What are the lead w...

https://www.ia.omron.com/support/faq/answer/34/faq00986/

FAQ00987 for Rotary Encoders | OMRON Industrial Au...

...s "Maximum response frequency"? Answer  The maximum frequency at which the signal can respond. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What are the lead w...

https://www.ia.omron.com/support/faq/answer/34/faq00987/

faq00994

...n somewhere is made to be understood in the axis and the chassis if there is no phase Z output. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What are the lead w...

https://www.ia.omron.com/support/faq/answer/34/faq00994/

FAQ00995 for Rotary Encoders | OMRON Industrial Au...

...) = Maximum response frequency ⁄ Resolution It is the rotation at which the signal can respond. E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What are the lead w...

https://www.ia.omron.com/support/faq/answer/34/faq00995/

FAQ00997 for Rotary Encoders | OMRON Industrial Au...

...tents Question How to mount the Rotary Encoder? Answer  The mounting procedures are as follow; E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What are the lead w...

https://www.ia.omron.com/support/faq/answer/34/faq00997/

FAQ01000 for Rotary Encoders | OMRON Industrial Au...

...table of possibility of connection. Yes: Possible No: Impossible Incremental Type Absolute Type E2E Standard Sensors for Detecting Ferrous Metals under Standard Conditions What are the lead w...

https://www.ia.omron.com/support/faq/answer/34/faq01000/

結果 1861 - 18804543

国/地域選択

Related Contents