Page top

Lead Contents

FAQ00900 of Timers FAQ

FAQ No. FAQ00900

Primary Contents


What is the method for turning the output ON and OFF at specific times for the whole year?


Use the H5S's cyclic operation function.

1. Press the Cycle/Pulse Key.

2. Select all the days of the week (Sunday to Saturday).

3. Set the cycle to start at AM 0:00.

4. Set the cycle to stop at PM 11:59.

5. Set the ON time length.

6. Set the OFF time length.

For the above settings, the output must be OFF for one minute starting at 11:59.

Starting and stopping from different times is also possible.

However, the ON time length and OFF time length combined must be divisible by 24 hours.

Recommended Products


A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current Signals


A New High-performance Controller: High Resolution, High Speed, and High Input Accuracy. Logic Operations and Preventive Maintenance Function.


Easy to Use and Easy to Read.

Other Timers FAQ