Page top

Lead Contents

FAQ03053 of Timers FAQ

FAQ No. FAQ03053

Primary Contents

Question

Is it possible for a Timer to continuously apply power?

Answer



Yes it is, but do not leave the Timer in a time-expired condition for long periods of time (e.g., a month or longer) under high-temperature conditions.

Doing so may reduce the life of the Timer due to deterioration of internal parts, such as electrolytic capacitors.

If the Timer is to be left in a timed-out status for extended periods of tie, use together with Relays in the following type of circuit.

(Written using JIS notation)

Recommended Products

K3HB-X

A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current Signals

E5CN-H

A New High-performance Controller: High Resolution, High Speed, and High Input Accuracy. Logic Operations and Preventive Maintenance Function.

H5CZ

Easy to Use and Easy to Read.

Other Timers FAQ