Page top

Lead Contents

FAQ03112 of Timers FAQ

FAQ No. FAQ03112

Primary Contents

Question

What is a substitute product for H3CR-A8EL Solid-state Timers?

Answer



The substitute productis H3CR-A8E. Because the length of the body is approximately 12 mm shorter than that of H3CR-A8EL, Y92H-8 Hold-down Clips should be used instead of Y92H-2 when using PF085A Sockets, and Y92H-7 Hold-down Clips should be used instead of Y92H-1 Hold-down Clips when using PL08 Sockets.
The power supply voltage specifications will be 100 to 240 VAC/100 to 125 VDC instead of 100 to 240 VAC.

Recommended Products

K3HB-X

A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current Signals

E5CN-H

A New High-performance Controller: High Resolution, High Speed, and High Input Accuracy. Logic Operations and Preventive Maintenance Function.

H5CZ

Easy to Use and Easy to Read.

Other Timers FAQ