Page top

Lead Contents

FAQ00718 of Level Switches FAQ

FAQ No. FAQ00718

Primary Contents

Question

What would be an appropriate 61F Floatless Level Controllers, Electrode Holders, and Electrodes for detecting the level of seawater?

Answer



Use a low-sensitivity 61F (one with the suffix D on the model number), BS-1T Electrode Holders (titanium), and F03-01 Electrodes (titanium).

If BS-1 or BF-1 Electrode Holders is used, the stainless-steel electrode nuts will corrode and have to be regularly replaced.

Also, allow at least 1 m of space between Electrodes.