Page top

Lead Contents

FAQ00733 of Level Switches FAQ

FAQ No. FAQ00733

Primary Contents

Question

Can two 61F Floatless Level Controllers and two Electrode Holders be used in the same tank?

Answer



Yes, they can as long as the following conditions are met.

The interelectrode voltages are the same.

The minimum separation between the Electrode Holders depends on the type of liquid, but separate the Electrode Holders by at least 1 m.

Use the same phases at the power supply terminals (S0, S1, and S2).