![]()
Global
These are navigation links to move inside this page.
Knob-type Selector Switch (Detachable) (Cylindrical 16-dia.)
Separate Construction with Cylindrical 16-dia. Body
![]()
Quick links OMRON IA Push Buttons / Indicator Lamps in your country.
Please contact Europe headquarters.
Rectangular A165[]-J
Solder terminals (tab terminals #110)
Square A165[]-A
Solder terminals (tab terminals #110)
Round A165[]-T
Solder terminals (tab terminals #110)
Rectangular A165[]-J
PCB terminals
The following diagrams show the rectangular model as a representative example.
The lamp terminal is also provided with non-lighted models.
Rectangular A165W[]-T
Reduced-voltage lighting solder terminals (tab terminals #110)
The following diagrams show the rectangular model as a representative example.
Rectangular A165[]-2S
Screw-Less Clamp
The following diagrams show the rectangular model as a representative example.
Panel Cutouts
Models with Solder Terminals and Models with Screw-less Clamp Connectors
Note:
1. Make sure the thickness of the mounting panel is 0.5 to 3.2 mm.
2. If the panel is to be finished with coating, etc., make sure that the panel meets the specified dimensions after coating.
3. Figures in parentheses are for screw-less clamp connectors.
Models with PCB Terminals
Note:
1. Ensure that the variation in the distance between the centers of neighboring mounting holes is less than ±0.1 mm.
2. Make sure the thickness of the mounting panel is 0.5 to 3.2 mm. If, however, a Switch Guard or Dust Cover is used, the thickness of the mounting panel must be 0.5 to 2 mm.
3. If the panel is to be finished with coating, etc., make sure that the panel meets the specified dimensions after coating.
Caution: All units are in millimeters unless otherwise indicated.