Page top

ZX2

Smart Sensors Laser Displacement Sensors CMOS Type

ZX2

Stable measurement that is unaffected by workpiece changes. The simple setting for everyone.

(Stability)
Stable measurements in case of color/material and moving objects

Dynamic range of two million times (PAT.P)

Stable measurements are enabled for any color or surface condition, including metals, substrates, elastomers, and transparent materials, through OMRON's unique HSDR-CMOS (High Speed and Dynamic Range) image sensor and a step-less laser power adjustment algorithm.


A line beam is used in addition to an emitter beam when dealing with rough surfaces to average out the amount of reflected light and to offset the amount of light received at a high-speed measurement period of 30 μs in order to reduce variations in received light and to enable stable measurements for moving objects.

CMOS Image Sensor

ZX2 Features 6 ZX2_Features1

Step-less adjustment of laser power

ZX2 Features 8 ZX2_Features2

Stable measurements on objects with changing color/material

ZX2 Features 10 ZX2_Features3

Stable measurements on moving objects

ZX2 Features 12 ZX2_Features4

(Easy)
Easy and User-friendly Configuration

Smart tuning (PAT.P)

The ideal configuration for stable measurements is realized by a single button through the new feature "smart tuning", and no longer depends on the skill of the user. A reliable configuration is achieved by three tuning methods, which can be selected to match the type of object and surface conditions to be measured.

ZX2 Features 16 ZX2_Features5

Three selectable tunings

ZX2 Features 18 ZX2_Features6

Single smart tuning

Best configuration for stable detection in case of objects do not change by pushing the button for one second

ZX2 Features 21 ZX2_Features7

Multi-smart tuning

Ideal configuration for stable detection of changing objects by pushing the button for three seconds

ZX2 Features 24 ZX2_Features8

Active smart tuning

Continuous configuration improvement for the stable detection of all locations by pushing the button for five seconds

Reliable measurements in harsh environments

IP67, robot cable & temperature characteristic 0.02% F.S./°C

IP67 protection class enables to use the sensor in harsh environments. A robot cable is used as standard between the head and amplifier, that the unit can be used reliably on moving parts. In addition, as 3D UV bond is used to fix the optical components rather than screws, stress can be controlled and a temperature characteristic 0.02% F.S./°C* is realized.

ZX2 Features 30 ZX2_Features9

Note:If the room temperature varies 1°C, the measured value varies 0.02% F.S. (corresponding to 4μm for the Model ZX2-LD50)

Compact sensor for easy mounting

World smallest*

The world's smallest CMOS laser displacement sensor head is realized in a resin case. Enables to mount the sensor in smallest spaces and to minimize measurement errors arising from temperature fluctuations.

ZX2 Features 35 ZX2_Features10

Note:According to OMRON investigation of CMOS laser displacement sensors performed in September 2010.

10μm precision measurements

Linearity to meet the application

Measurements to an even higher accuracy are realized for applications that do not require the entire measurement range. If the range of the field is less than the length of the measurement center, linearity accuracy improves by 50% compared with that for the full range.*

ZX2 Features 40 ZX2_Features11

Note:For the ZX2-LD50L/LD100L.

Visualization to prevent from stopping the production-line

Laser life display function

The end of the laser diode lifespan is automatically detected and displayed so maintenance can be performed systematically. On the main digital display of the amplifier, this is indicated by an LED on the back of the head. Accordingly, in case of amplifier is within the control panel, the lifetime can be confirmed by the head and the indications are not missed.

ZX2 Features 45 ZX2_Features12

No need for a manual

11 Segment LED Display

An 11 segment LED display is integrated in the compact housing. Alphanumeric characters can be read with ease and there is no need to refer to a manual.

Comparison of the existing 7 segment LED display and the 11 segment LED display

ZX2 Features 50 ZX2_Features13
ZX2 Features 51 ZX2_Features14

Perform two calculations with ease

Thickness + subtraction mode

The calculated results of two sensor heads are displayed on the amplifier unit by just connecting the calculating unit between the two amplifier units. The calculation function can be chosen from the two modes of thickness and subtraction. It is also possible to prevent mutual interference by coupling via the calculating units. (Up to five amplifier units can be connected.)

Thickness mode

Note:

ZX2 Features 56 ZX2_Features15

Subtraction mode

ZX2 Features 58 ZX2_Features16

Easy change of setup

Equipped with 4 banks

The amplifier unit is equipped with four bank functions.
Easy change of setup between four modes is supported by just switching between the bank functions.

ZX2 Features 62 ZX2_Features17