Page top


NX-series Pulse Output Unit


Positioning with Pulse Input Type Motor Drivers Such As Stepper Motor Drive

When the motion control instructions of the MC Function Modules of the NJ/NX/NY5-series Machine Automation Controller are used, number of usable units is the same as the maximum number of axes controlled by the NJ/NX/NY5-series Controller.

High-speed remote I/O control with communications cycle as fast as 125 μs.*1

Synchronous I/O refreshing or Task Period Prioritized refreshing *2, can be selected for refreshing with the NX-series EtherCAT Coupler.

Latch function (2 external latch inputs)

Open collector pulse outputs up to 500 kHz or line driver pulse outputs up to 4 MHz.

Line driver output models with two or four channels.

Connection to the CJ-series is possible by connecting with the EtherNet/IPTM Coupler.

*1. When using the NX-EC01[][] together with the NX701-[][][][] and NX-ECC203.
*2. Task Period Prioritized refreshing is available when the NX-ECC203 is used together.

Sysmac is a trademark or registered trademark of OMRON Corporation in Japan and other countries for OMRON factory automation products.
EtherCAT® is a registered trademark of Beckhoff Automation GmbH for their patented technology. EtherNet/IPTM is the trademarks of ODVA.
Other company names and product names in this document are the trademarks or registered trademarks of their respective companies.