The opening does not obstruct the airflow from the Air Clean Unit eliminating worries about disrupting the laminar airflow.
Ionizers for Air Clean Unit
             
        
last update: December 19, 2013
 
       
       
    The opening does not obstruct the airflow from the Air Clean Unit eliminating worries about disrupting the laminar airflow.
 
       
       
    Variale DC ionization is used to discharge over a wide area.
Two Sensors provide constant feedback on the ion balance to maintain uniform discharging.
 
       
       
    LED indicators and external outputs provide notification when discharge needles require cleaning or discharge errors occur. Cleaning outputs are made at two levels: warnings and alarms.
 
       
       
    Discharging is stopped when a signal indicating that the Air Clean Unit fan has stopped is received. This function prevents ozone from remaining due to discharging.
 
       
       
    Discharge needles are modular and can be easily replaced.
 
       
       
    The Ionizer can be installed easily by inserting it between the Air Clean Unit and the top of the Clean Booth and securing it with screws. Wiring work is greatly reduced by the connectors used for connection to the Air Clean Units.
 
       
       
    last update: December 19, 2013