A ball spline mechanism is used to hold the balls in grooves (on the right in the following diagram). This helps prevent the balls from damaging internal parts due to vibration or shock to reduce the chance of malfunction. In comparison with the previous method (on the left in the following diagram), load capacity is increased and an exceptionally smooth sliding operation is achieved for long-term stable operation.