Page top

H7CC-R

Digital Tachometer

H7CC-R

New and improved design for easier use, setting and maintenance. The improved user interface is intuitive and offers better overall visibility. Replacement time notification function notifies the user of potential preventive maintenance

Software Download

You can download software for the H7CC.

(Unit: mm)

Tachometers

Dimensions without Flush Mounting Adapter
H7CC-R[]

H7CC-R Dimensions 2

Dimensions with Flush Mounting Adapter
(Adapter and Waterproof Packing Ordered Separately)
H7CC-R[]

H7CC-R Dimensions 3

Panel Cutouts

Panel cutouts are as shown below (according to DIN43700).

H7CC-R Dimensions 4

Note:
1. The mounting panel thickness should be 1 to 5 mm.
2. To allow easier operation, it is recommended that Adapters be mounted so that the gap between sides with hooks is at least 15 mm (i.e., with the panel cutouts separated by at least 60 mm).
3. It is possible to horizontally mount Timers side by side. Attach the Flush Mounting Adapters so that the surfaces without hooks are on the sides of the Timers. If Counters/Tachometers are mounted side by side, however, water resistance will be lost.

H7CC-R Dimensions 5

Dimensions with Front Connecting Socket
H7CC-R[]

H7CC-R Dimensions 6

Accessories (Order Separately)

Note: Depending on the operating environment, the condition of resin products may deteriorate, and may shrink or become harder. Therefore, it is recommended that resin products are replaced regularly.

Soft Cover
Y92A-48F1

H7CC-R Dimensions 8

Hard Cover
Y92A-48

H7CC-R Dimensions 9

Protecting the Counter/Tachometer in Environments Subject to Oil

The H7CC's panel surface is water-resistive (conforming to IP[]6) and so even if drops of water penetrate the gaps between the keys, there will be no adverse effect on internal circuits. If, however, there is a possibility of oil being present on the operator's hands, use the Soft Cover. The Soft Cover ensures protection equivalent to IP54F against oil. Do not, however, use the H7CC in locations where it would come in direct contact with oil.

Waterproof Packing
Y92S-P6

H7CC-R Dimensions 11

Note: The Waterproof Packing is included with models with screw terminals.
Order the Waterproof Packing separately if it is lost or damaged. The Waterproof Packing can be used to achieve IP66 protection.

The panel surface of the H7CC-A/-R is water-resistant (conforming to IP66). To protect the internal circuits from water penetration through the space between the H7CC and operating panel, waterproof packing is included. Attach the Y92F-30 Adapter with sufficient pressure with the reinforcing screws so that water does not penetrate the panel.

H7CC-R Dimensions 13

The Waterproof Packing will deteriorate, harden, and shrink depending on the application environment. To ensure maintaining the IP[]6 waterproof level, periodically replace the Waterproof Packing.
The periodic replacement time will depend on the application environment. You must confirm the proper replacement time. Use 1 year or less as a guideline. If the Waterproof Packing is not replaced periodically, the waterproof level will not be maintained. It is not necessary to mount the Waterproof Packing if waterproof construction is not required.

Flush Mounting Adapter
Y92F-30

H7CC-R Dimensions 15

Order the Flush Mounting Adapter with the following model number separately if it is lost or damaged.
Note: The Waterproof Packing is included with models with screw terminals.

Y92F-45

Note:
1. The adapter is black in color.
2. The Y92F-45 can be used in combination with the Y92F-30 Adapter provided with the Counter.

H7CC-R Dimensions 17

H7CC Mounting Example

H7CC-R Dimensions 18

Connection Sockets

Front Connecting Socket

P2CF-11

H7CC-R Dimensions 21

P2CF-11-E
(Finger-safe Type)

H7CC-R Dimensions 22

P2CF-08

H7CC-R Dimensions 23

P2CF-08-E
(Finger-safe Type)

H7CC-R Dimensions 24

Note: Round crimp terminals cannot be used on Finger-safe Sockets. Use forked crimp terminals.

Back-connecting Sockets

P3GA-11

H7CC-R Dimensions 27

P3G-08

H7CC-R Dimensions 28

Note: A Y92A-48G Terminal Cover can be used with the Socket to create a finger-safe construction.

Terminal Covers for P3G-08/P3GA-11 Back-connecting Socket

Y92A-48G

H7CC-R Dimensions 31

Note: The Terminal Cover can be used with a Back-mounting Socket (P3GA-11, P3G-08) to create a finger-safe construction.

Optional Products for Track Mounting

Mounting Track
PFP-100N
PFP-50N

H7CC-R Dimensions 34

Mounting Track
PFP-100N2

H7CC-R Dimensions 35

End Plate
PFP-M

H7CC-R Dimensions 36

Spacer
PFP-S

H7CC-R Dimensions 37

Note: Order Spacers in increments of 10.