(Unit: mm)
Digital Timer
You can download software for H5CC
last update: May 11, 2026
(Unit: mm)
H5CC-A/-AD/-AS/-ASD/-AU/-AUD/-AWSD (Flush Mounting Models)
Note: M3.5 terminal screw (effective length: 6 mm)
H5CC-A11/-A11D/-A11F/-A11S/-A11SD (Flush Mounting/Surface Mounting Models)
H5CC-L8/-L8D/-L8S/-L8SD/-L8E/-L8ED/-L8EF (Flush Mounting/Surface Mounting Models)
H5CC-A/-AD/-AS/-ASD/-AU/-AUD/-AWSD (Flush Mounting Models)
(Provided with Adapter and Waterproof Packing)
H5CC-L8/-L8D/-L8S/-L8SD/-L8E/-L8ED-A11/-A11D/-A11F/-A11S/-A11SD (Flush Mounting Models)
(Adapter and Waterproof Packing Ordered Separately)
Panel cutouts are as shown below. (According to DIN 43700.)
Note: 1. The mounting panel thickness should be 1 to 5 mm.
Note: 2. To allow easier operation, it is recommended that Adapters be mounted so that the gap between sides with hooks is at least 15 mm (i.e., with the panel cutouts separated by at least 60 mm).
Note: 3. It is possible to horizontally mount Timers side by side. Attach the Flush Mounting Adapters so that the surfaces without hooks are on the sides of the Timers. If they are mounted side-by-side, water resistance will be lost.
* These dimensions depend on the kind of DIN track and Sockets. (Reference value.)
Note: Depending on the operating environment, the condition of resin products may deteriorate, and may shrink or become harder. Therefore, it is recommended that resin products are replaced regularly.
Soft Cover
Y92A-48F1
The Soft Cover is attached by inserting the front part between the holding clips.
Hard Cover
Y92A-48
Note: Due to material properties, the product surface may become cloudy white. If this causes any issues during use, please wipe it with isopropyl alcohol or similar before using.
The H5CC’s panel surface is water-resistive (IP[]6) and so even if drops of water penetrate the gaps between the keys, there will be no adverse effect on internal circuits. If, however, there is a possibility of oil being present on the operator’s hands, use the Soft Cover. The Soft Cover ensures protection equivalent to IP54 against oil. Do not, however, use the H5CC in locations where the front section would come in direct contact with oil.
Waterproof Packing
Y92S-P6
* The Waterproof Packing is included with models with screw terminals.
Order the Waterproof Packing separately if it is lost or damaged.
The Waterproof Packing can be used to achieve IP66 protection.
The Waterproof Packing will deteriorate, harden, and shrink depending on the application environment. To ensure maintaining the IP[]6 waterproof level, periodically replace the Waterproof Packing.
The periodic replacement period will depend on the application environment. You must confirm the proper replacement period. Use one year or less as a guideline. If the Waterproof Packing is not replaced periodically, the waterproof level will not be maintained.
It is not necessary to mount the Waterproof Packing if waterproof construction is not required.
Flush Mounting Adapter
Y92F-30
Order the Flush Mounting Adapter separately if it is lost or damaged.
Note: A Flush Mounting Adapter is included with models with screw terminals.
Y92F-38
* Insert the timer unit from front side of adapter.
* Use Waterproof Packing to provide a level of water protection that complies with IP[]6 standards.
* It is not necessary to mount the Waterproof Packing if waterproof construction is not required.
Waterproof Packing
Y92S-35
The Y92S-35 is not provided with the Y92F-38. Order separately, if water protection is required. Use Waterproof Packing to provide a level of water protection that complies with IP65 standards.
Depending on the operating environment, the Waterproof Packing may deteriorate, contract, or harden and so regular replacement is recommended. The periodic replacement period will depend on the application environment. You must confirm the proper replacement period. Use one year or less as a guideline. If the Waterproof Packing is not replaced periodically, the waterproof level will not be maintained.
Y92F-45
Note: 1. The adapter is black in color.
Note: 2. The Y92F-45 can be used in combination with the Y92F-30 Adapter provided with the Timer.
H5CC Mounting Example
P2CF-08
P2CF-08-E
(Finger-safe Type)
P2CF-11
P2CF-11-E
(Finger-safe Type)
Note: Round crimp terminals cannot be used on Finger-safe Sockets. Use forked crimp terminals.
The P2CF has hooks to fix the timer so the holding clips are not required.
P3G-08
P3GA-11
Note: A Y92A-48G Terminal Cover can be used with the Socket to enable finger protection.
Y92A-48G
Note: The Terminal Cover can be used with a Back Connecting Socket (P3G-08 or P3GA-11) to enable finger protection.
Mounting Track
PFP-100N
PFP-50N
Mounting Track
PFP-100N2
End Plate
PFP-M
Spacer
PFP-S
Note: Order Spacers in increments of 10. The above prices are the standard prices for one item.
last update: May 11, 2026